<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can MMPF0100F0AEP VGEN6 supplies to VIN1? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-MMPF0100F0AEP-VGEN6-supplies-to-VIN1/m-p/442720#M68063</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about MMPF100F0AEP.&lt;/P&gt;&lt;P&gt;Actually, our partner consider using MMPF0100F0AEP VGEN6 (3.3V) for VGEN1 supply.&lt;/P&gt;&lt;P&gt;I think VGEN6 output voltage accuracy (+-3%) is good to supply VGEN1 (up to 3.40V input) since 3.3V * 103% = 3.399V.&lt;/P&gt;&lt;P&gt;And I think there is no timing issue since VGEN6 turn-on time is up to 500 us, it is sufficient to supply VGEN1 (SEQ=9) from VGEN6 (SEQ=8).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I have concern about start-up overshoot.&lt;/P&gt;&lt;P&gt;VGEN6's start-up overshoot(max) is 2.0%, so in worst case, VGEN6 voltage will be 3.3V * 103%(voltage accuracy) * 102% (start-up overshoot) = 3.47V.&lt;/P&gt;&lt;P&gt;It exceeds VIN1 input voltage (up to 3.4V).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, in the case of SW4 which is used for VIN1 supply on SABRE-SD, it also exceeds VIN1 input voltage in worst case as following.&lt;/P&gt;&lt;P&gt;3.15V * 106% (in PWM mode) + 66mV (start-up overshoot) = 3.405V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I'm confused by these calculation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;/P&gt;&lt;P&gt;Can we use VGEN6 to supply VIN1?&lt;/P&gt;&lt;P&gt;How should we judge whether each MMPF0100F0AEP output can supply to VIN1 or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jun 2015 07:20:56 GMT</pubDate>
    <dc:creator>satoshishimoda</dc:creator>
    <dc:date>2015-06-30T07:20:56Z</dc:date>
    <item>
      <title>Can MMPF0100F0AEP VGEN6 supplies to VIN1?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-MMPF0100F0AEP-VGEN6-supplies-to-VIN1/m-p/442720#M68063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about MMPF100F0AEP.&lt;/P&gt;&lt;P&gt;Actually, our partner consider using MMPF0100F0AEP VGEN6 (3.3V) for VGEN1 supply.&lt;/P&gt;&lt;P&gt;I think VGEN6 output voltage accuracy (+-3%) is good to supply VGEN1 (up to 3.40V input) since 3.3V * 103% = 3.399V.&lt;/P&gt;&lt;P&gt;And I think there is no timing issue since VGEN6 turn-on time is up to 500 us, it is sufficient to supply VGEN1 (SEQ=9) from VGEN6 (SEQ=8).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I have concern about start-up overshoot.&lt;/P&gt;&lt;P&gt;VGEN6's start-up overshoot(max) is 2.0%, so in worst case, VGEN6 voltage will be 3.3V * 103%(voltage accuracy) * 102% (start-up overshoot) = 3.47V.&lt;/P&gt;&lt;P&gt;It exceeds VIN1 input voltage (up to 3.4V).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, in the case of SW4 which is used for VIN1 supply on SABRE-SD, it also exceeds VIN1 input voltage in worst case as following.&lt;/P&gt;&lt;P&gt;3.15V * 106% (in PWM mode) + 66mV (start-up overshoot) = 3.405V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I'm confused by these calculation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;/P&gt;&lt;P&gt;Can we use VGEN6 to supply VIN1?&lt;/P&gt;&lt;P&gt;How should we judge whether each MMPF0100F0AEP output can supply to VIN1 or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 07:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-MMPF0100F0AEP-VGEN6-supplies-to-VIN1/m-p/442720#M68063</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2015-06-30T07:20:56Z</dc:date>
    </item>
    <item>
      <title>Re: Can MMPF0100F0AEP VGEN6 supplies to VIN1?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-MMPF0100F0AEP-VGEN6-supplies-to-VIN1/m-p/442721#M68064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use VGEN6 to supply VIN1, since&lt;/P&gt;&lt;P&gt;VIN1 is rated up to 3.6V, 3.40V is specified data for permanent&lt;/P&gt;&lt;P&gt;operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="MMPF0100  p.8.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61060i5DDF77032D088049/image-size/large?v=v2&amp;amp;px=999" role="button" title="MMPF0100  p.8.jpg" alt="MMPF0100  p.8.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2015 09:10:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-MMPF0100F0AEP-VGEN6-supplies-to-VIN1/m-p/442721#M68064</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-30T09:10:10Z</dc:date>
    </item>
    <item>
      <title>Re: Can MMPF0100F0AEP VGEN6 supplies to VIN1?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-MMPF0100F0AEP-VGEN6-supplies-to-VIN1/m-p/442722#M68065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;OK, I understood it is no problem even though the input voltage exceed 3.40V momentarily.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 10:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-MMPF0100F0AEP-VGEN6-supplies-to-VIN1/m-p/442722#M68065</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2015-07-01T10:43:38Z</dc:date>
    </item>
  </channel>
</rss>