<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX281 CAN Bus output</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442389#M68008</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, I understand, thank you!:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Sep 2015 02:47:26 GMT</pubDate>
    <dc:creator>annyli</dc:creator>
    <dc:date>2015-09-15T02:47:26Z</dc:date>
    <item>
      <title>IMX281 CAN Bus output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442386#M68005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The CAN_RX and CAN_TX can be connected to the CAN chip directly in my opinion. So why the EVK board use a buffer chip before CAN chip? Is it necessary?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 06:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442386#M68005</guid>
      <dc:creator>annyli</dc:creator>
      <dc:date>2015-09-11T06:54:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX281 CAN Bus output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442387#M68006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Buffers are used as level shifter (3.3V to 5V and 5V to 3.3V) if You use a 3.3V CAN-Bus Transceiver (for example SN65HVD232 from TI) they are not needed, or if You use a 5V type with TTL Inputs, You only have to reduce the RX output to 3.3V level .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 09:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442387#M68006</guid>
      <dc:creator>MartinHo</dc:creator>
      <dc:date>2015-09-11T09:49:38Z</dc:date>
    </item>
    <item>
      <title>Re: IMX281 CAN Bus output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442388#M68007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi anny&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right: they can be connected directly.&lt;/P&gt;&lt;P&gt;EVK board was designed to provide as much possible connections&lt;/P&gt;&lt;P&gt;as possible to test all available interfaces and its options.&lt;/P&gt;&lt;P&gt;These buffers were added for flexibility,&amp;nbsp; for example MX28 EVK board supports&lt;/P&gt;&lt;P&gt;up to 4 NAND flash ICs (CE0, CE1, CE2, and CE3).&lt;/P&gt;&lt;P&gt;However, the 0 ohm options for CE2 and CE3 are disconnected by&lt;/P&gt;&lt;P&gt;default (they are used for CAN).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Sep 2015 11:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442388#M68007</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-11T11:27:21Z</dc:date>
    </item>
    <item>
      <title>Re: IMX281 CAN Bus output</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442389#M68008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, I understand, thank you!:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Sep 2015 02:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX281-CAN-Bus-output/m-p/442389#M68008</guid>
      <dc:creator>annyli</dc:creator>
      <dc:date>2015-09-15T02:47:26Z</dc:date>
    </item>
  </channel>
</rss>