<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: which u-boot version supports for imx6dl board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442350#M68003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;sdc is not a partition but the raw disk. The offset is because the partition table will start from 0, so u-boot need to reside after that.&lt;/P&gt;&lt;P&gt;I'd recommend to create a partition for your file system at offset 16MiB from the start of the disk, that way you should also be sure that u-boot don't share a flash erase block with the file system, thus less likely to corrupt u-boot during a power outage for instance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Use e.g. Gparted for creating the partition for the file system at the right offset, then "dd if=u-boot.imx of=/dev/sdc bs=1k seek=1", and you should be good to go.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Apr 2015 07:29:28 GMT</pubDate>
    <dc:creator>ThomasG1z</dc:creator>
    <dc:date>2015-04-29T07:29:28Z</dc:date>
    <item>
      <title>which u-boot version supports for imx6dl board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442345#M67998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi i.mx community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can any one tell me which version of u-boot supports for i.mx6dl board&lt;/P&gt;&lt;P&gt;and depending upon this board i am making my custom board for that also send detailed procedure to modify uboot for my board&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance&lt;/P&gt;&lt;P&gt;happy weekend&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2015 11:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442345#M67998</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-04-24T11:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: which u-boot version supports for imx6dl board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442346#M67999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi saida&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uboot version can be found in i.MX_Linux_Release_Notes.pdf&lt;/P&gt;&lt;P&gt;included in documents &lt;A href="https://www.freescale.com/webapp/Download?colCode=L3.14.28_1.0.0_LINUX_DOCS&amp;amp;location=null&amp;amp;fasp=1&amp;amp;WT_TYPE=Supporting%20Information&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=gz&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.gz"&gt;L3.14.28_1.0.0_LINUX_DOCS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For modifications one can look at i.MX_6_BSP_Porting_Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2015 12:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442346#M67999</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-04-24T12:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: which u-boot version supports for imx6dl board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442347#M68000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for your reply&lt;/P&gt;&lt;P&gt;i gone through that document which shows that u-boot-2014.04 is supporting version&lt;/P&gt;&lt;P&gt;i downloaded source code and i have done following steps&lt;/P&gt;&lt;P&gt;$ tar xzf u-boot-2014.04.tar.bz&lt;/P&gt;&lt;P&gt;$ cd u-boot&lt;/P&gt;&lt;P&gt;$ make mx6dlsabresd_config (it was showing some nitrogenxl and config for mx6dlsabresd board)&lt;/P&gt;&lt;P&gt; generated u-boot.imx file than&lt;/P&gt;&lt;P&gt;$ dd if=u-boot.imx of=/dev/sdc1 bs=1k seek=1&lt;/P&gt;&lt;P&gt;$sync&lt;/P&gt;&lt;P&gt;i inserted in sdcard slot but its unable to boot&lt;/P&gt;&lt;P&gt;please help in this regard&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2015 11:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442347#M68000</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-04-28T11:54:04Z</dc:date>
    </item>
    <item>
      <title>Re: which u-boot version supports for imx6dl board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442348#M68001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I assume you don't want to dd to partition 1 on sdc disk, but /dev/sdc itself, or the offset will be wrong. And if you also have the rootfs on this disk make sure you have enough space for u-boot (and perhaps the environment depending on where you store that) before the rootfs partition starts (e.g. sdc1), start at e.g. 16MiB offset for that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Apr 2015 14:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442348#M68001</guid>
      <dc:creator>ThomasG1z</dc:creator>
      <dc:date>2015-04-28T14:08:46Z</dc:date>
    </item>
    <item>
      <title>Re: which u-boot version supports for imx6dl board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442349#M68002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you&amp;nbsp; for reply&lt;/P&gt;&lt;P&gt;when i insert sdcard through usb adapter in /dev/ there are&amp;nbsp; two partions its showing sdc,sdc1 may be i selected wrong one(that is sdc1)&lt;/P&gt;&lt;P&gt;can you give the details of how sdcard should be formated and why the offset is at 1024 bytes address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 05:59:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442349#M68002</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-04-29T05:59:57Z</dc:date>
    </item>
    <item>
      <title>Re: which u-boot version supports for imx6dl board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442350#M68003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;sdc is not a partition but the raw disk. The offset is because the partition table will start from 0, so u-boot need to reside after that.&lt;/P&gt;&lt;P&gt;I'd recommend to create a partition for your file system at offset 16MiB from the start of the disk, that way you should also be sure that u-boot don't share a flash erase block with the file system, thus less likely to corrupt u-boot during a power outage for instance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Use e.g. Gparted for creating the partition for the file system at the right offset, then "dd if=u-boot.imx of=/dev/sdc bs=1k seek=1", and you should be good to go.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 07:29:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442350#M68003</guid>
      <dc:creator>ThomasG1z</dc:creator>
      <dc:date>2015-04-29T07:29:28Z</dc:date>
    </item>
    <item>
      <title>Re: which u-boot version supports for imx6dl board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442351#M68004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;its working when i did dd on sdc&lt;/P&gt;&lt;P&gt;thank you thomas its very helpful and i am following posts to port linux kernel,root filesystem if anything required i will come back to you&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp; much&lt;/P&gt;&lt;P&gt;byee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 08:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/which-u-boot-version-supports-for-imx6dl-board/m-p/442351#M68004</guid>
      <dc:creator>saida</dc:creator>
      <dc:date>2015-05-05T08:34:23Z</dc:date>
    </item>
  </channel>
</rss>