<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Issue About Power Manager on MX6DL</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Issue-About-Power-Manager-on-MX6DL/m-p/442033#M67961</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor will exit from low power mode if there is&lt;/P&gt;&lt;P&gt;enabled interrupt from some peripheral.&lt;/P&gt;&lt;P&gt;You can try to find it probably disabling some of them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2015 00:41:51 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-10T00:41:51Z</dc:date>
    <item>
      <title>Issue About Power Manager on MX6DL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-About-Power-Manager-on-MX6DL/m-p/442032#M67960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I find a strange problem that when our board entered into sleep,from the log ,we found that once the board "sabresd_suspend_enter" then "sabresd_suspend_exit",why? log is following:&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.386809] ----suspend_enter----&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.387652] ---------max_timeout:0-----------&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.387658] power_suspend_late return 0&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.387668] PM: late suspend of devices complete after 0.847 msecs&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.387675] Disabling non-boot CPUs ...&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.388498] CPU1: shutdown&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.389154] ----syscore_suspend----&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.389292] -----sabresd_suspend_enter--------&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.389589] -----sabresd_suspend_exit--------&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.389833] Enabling non-boot CPUs ...&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.410766] CPU1: Booted secondary processor&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.410782] Calibrating delay loop (skipped) already calibrated this CPU&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.411156] i.MXC CPU frequency driver&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.411203] CPU1 is up&lt;/P&gt;&lt;P&gt;[&amp;nbsp; 131.411800] PM: early resume of devices complete after 0.586 msecs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And this log has entered into suspend. You can see maybe it has exit suspend ? why?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 12:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-About-Power-Manager-on-MX6DL/m-p/442032#M67960</guid>
      <dc:creator>tony_l_cai</dc:creator>
      <dc:date>2015-06-09T12:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: Issue About Power Manager on MX6DL</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Issue-About-Power-Manager-on-MX6DL/m-p/442033#M67961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi tony&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;processor will exit from low power mode if there is&lt;/P&gt;&lt;P&gt;enabled interrupt from some peripheral.&lt;/P&gt;&lt;P&gt;You can try to find it probably disabling some of them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2015 00:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Issue-About-Power-Manager-on-MX6DL/m-p/442033#M67961</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-10T00:41:51Z</dc:date>
    </item>
  </channel>
</rss>