<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Change PHY type in sabresd project in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442002#M67952</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll look at the information and see if I can get any more info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Dec 2015 17:19:26 GMT</pubDate>
    <dc:creator>niklasmolin</dc:creator>
    <dc:date>2015-12-03T17:19:26Z</dc:date>
    <item>
      <title>Change PHY type in sabresd project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442000#M67950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm upgrading the linux image from branch Daisy to Jethro for our board, using Sabresd machine as reference.&lt;/P&gt;&lt;P&gt;But it seems like it can't find the PHY (Vitesse) on our board, getting message:&lt;/P&gt;&lt;P&gt;fec 2188000.ethernet eth0: no PHY, assuming direct connection to switch&lt;/P&gt;&lt;P&gt;and the PHY mask (when it searches for the PHY, is set to 0xFFFFFFFF (printed in function fec_enet_mii_probe)&lt;/P&gt;&lt;P&gt;In the Daisy branch version, it had no problem to detect the PHY.&lt;/P&gt;&lt;P&gt;Is there some changes I need for this in the device tree file or some other config file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Niklas &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Nov 2015 17:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442000#M67950</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2015-11-25T17:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: Change PHY type in sabresd project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442001#M67951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Niklas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe no need to device tree changes. One can try to debug in linux or uboot,&lt;/P&gt;&lt;P&gt;adding printfs and comparing with working version. Also one can try to use&lt;/P&gt;&lt;P&gt;L3.14.38_6ul_LINUX_DOCS (REV L3.14.38_6ul) &lt;/P&gt;&lt;P&gt;GZ (3.4 MB) L3.14.38_6UL_LINUX_DOCS&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx-6-processors/i.mx6qp/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK?fpsp=1&amp;amp;tab=Documentation_Tab" rel="nofollow"&gt;http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.mx-6-processors/i.mx6qp/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK?fpsp=1&amp;amp;tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Dec 2015 01:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442001#M67951</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-12-01T01:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: Change PHY type in sabresd project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442002#M67952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll look at the information and see if I can get any more info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Niklas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 17:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442002#M67952</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2015-12-03T17:19:26Z</dc:date>
    </item>
    <item>
      <title>Re: Change PHY type in sabresd project</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442003#M67953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I finally had some time to go back and look at this again.&lt;/P&gt;&lt;P&gt;Find an issue in my device tree file.&lt;/P&gt;&lt;P&gt;Included phy = &amp;lt;&amp;amp;phy0&amp;gt;; when setting up the fec.&lt;/P&gt;&lt;P&gt;When I removed this, it scanned through all PHY's and found the PHY located on ID 0.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Feb 2016 20:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Change-PHY-type-in-sabresd-project/m-p/442003#M67953</guid>
      <dc:creator>niklasmolin</dc:creator>
      <dc:date>2016-02-10T20:46:16Z</dc:date>
    </item>
  </channel>
</rss>