<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX6SX's DDR3L consumption</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441906#M67937</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antoine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if M4 is accessing DDR, so for measurements boot only A9 core.&lt;/P&gt;&lt;P&gt;According to DDR3 specification memory goes to self-refresh&lt;/P&gt;&lt;P&gt;putting CKE low, i.MX6SX MMDC asserts it low automatically, this is described&lt;/P&gt;&lt;P&gt;in sect.40.4.6.2 Self refresh SoloX Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jul 2015 01:39:38 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-07-27T01:39:38Z</dc:date>
    <item>
      <title>iMX6SX's DDR3L consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441905#M67936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello every one,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently measuring the iMX6SX's consumption on the iMX6SX-sabreSD board. With the application note AN5050 about power consumption, I've managed to enter into the deep-sleep mode and the system idle mode.&lt;/P&gt;&lt;P&gt;I've also put resitors of 20mΩ at the different measuring points in order to measure the voltage drop over those points, and to determine the power consumption. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VDDARM_SOC_IN and VDDHIGH_IN's power data are nearly the same as Freescale's but the DDR3L isn't at all.&lt;/P&gt;&lt;P&gt; It's written in the AN that the power consumption should be around 22 mW for the DDR3L I/F + memories but in my case, it uses 500 mW.&lt;/P&gt;&lt;P&gt;I think that even if the system is in DSM or Idle mode, the DDR3L aren't in self refresh state.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know how to force the DDR3L to be in this mode of self-refresh ? Is there another command to add? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Antoine CHARON&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #505050; font-family: tahoma,arial,helvetica,sans-serif; font-size: 10pt;"&gt;PS: I'm using the Linux Version 3.10.53-1.10_ga+g496fbe0 provided by Freescale with the board&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2015 13:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441905#M67936</guid>
      <dc:creator>tonioch</dc:creator>
      <dc:date>2015-07-24T13:49:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX's DDR3L consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441906#M67937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antoine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check if M4 is accessing DDR, so for measurements boot only A9 core.&lt;/P&gt;&lt;P&gt;According to DDR3 specification memory goes to self-refresh&lt;/P&gt;&lt;P&gt;putting CKE low, i.MX6SX MMDC asserts it low automatically, this is described&lt;/P&gt;&lt;P&gt;in sect.40.4.6.2 Self refresh SoloX Reference Manual&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf" title="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf"&gt;http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2015 01:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441906#M67937</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-27T01:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX's DDR3L consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441907#M67938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for you answer. I tried to do the measurement without the M4 booted, but the problem remains..&lt;/P&gt;&lt;P&gt;Memory doesn't go in self-refresh automatically in my case, do you know if it exists some procedure to do it manually? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Antoine&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2015 15:18:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441907#M67938</guid>
      <dc:creator>tonioch</dc:creator>
      <dc:date>2015-07-27T15:18:48Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX's DDR3L consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441908#M67939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antoine&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;below detailed steps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57966iB4B6C28CA9D98901/image-size/large?v=v2&amp;amp;px=999" title="MX6SX power measurements.jpg" alt="MX6SX power measurements.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2015 15:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441908#M67939</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-27T15:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: iMX6SX's DDR3L consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441909#M67940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes that's exactly what I did. I've replaced all the shunts and other 0Ω resistors you mentionned in your document by 20 mΩ precision resistors.&lt;/P&gt;&lt;P&gt;After I entered the command for DSM, I have exactly the same messages coming back from UART.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only consumption differences are for the two precision resistors R373 (DDR3L) and SH7 (SYS_3V8).&lt;/P&gt;&lt;P&gt;From the first (R373), I measured 7.535 mV, so the memories are using 497 mW. &lt;/P&gt;&lt;P&gt;From the second (SH7), I measured 5.044 mV, so the SYS_3V8 power rail is using 958 mW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the same board (&lt;EM&gt;SCH-27962 Rev. C&lt;/EM&gt;), but I don't use exactly the same SW Image (&lt;EM style="color: #505050; font-size: 10pt; font-family: tahoma,arial,helvetica,sans-serif;"&gt;3.10.53-1.10_ga+g496fbe0). &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #505050; font-family: tahoma,arial,helvetica,sans-serif; font-size: 10pt;"&gt;Do you think the problem could come from that sofware's difference? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #505050; font-family: tahoma,arial,helvetica,sans-serif; font-size: 10pt;"&gt;Sincerely,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #505050; font-family: tahoma,arial,helvetica,sans-serif; font-size: 10pt;"&gt;Antoine&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 08:38:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX6SX-s-DDR3L-consumption/m-p/441909#M67940</guid>
      <dc:creator>tonioch</dc:creator>
      <dc:date>2015-07-28T08:38:47Z</dc:date>
    </item>
  </channel>
</rss>