<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX6 Asynchronous Audmux/SSI</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Asynchronous-Audmux-SSI/m-p/441329#M67811</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having trouble getting SSI to work in asynchronous, 2 channel, network mode on the imx6 platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried using ssi as both a master and slave.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Master:&lt;/P&gt;&lt;P&gt;In the master configuration when i enable transmit I can see a correctly generated bit clk and frame sync present on the output of the audmux (port 4).&lt;/P&gt;&lt;P&gt;However&amp;nbsp; the same bit clk and frame sync is present on the receive lines even though the ssi controller, and both ports on the audmux are set to asynchronous.&lt;/P&gt;&lt;P&gt;There is no rx frame sync interrupt generated to the ssi controller however, and the txfs interrupt is fired only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i enable receive in this configuration instead, nothing comes out of the audmux on the receive or transmit lines, but the receive frame sync interrupt for the ssi controller is fired.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This lead me to believe the audmux was configured incorrectly, but other than disabling sync on that and setting the correct ports there doesn't to be anything else to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR1: 00006000&lt;/P&gt;&lt;P&gt;PTCR1: 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR4: 00000000&lt;/P&gt;&lt;P&gt;PTCR4: 84210000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Slave:&lt;/P&gt;&lt;P&gt;I have been unable to get this to work at all, no matter the configuration that I use, synchronous or otherwise.&lt;/P&gt;&lt;P&gt;Unfortunately asynchronous slave is the ideal mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I have the audmux settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR1: 00006000&lt;/P&gt;&lt;P&gt;PTCR1: 9ce73000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR4: 00000000&lt;/P&gt;&lt;P&gt;PTCR4: 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I never get any form of frame sync interrupt no matter what I feed in.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jun 2015 21:29:41 GMT</pubDate>
    <dc:creator>nathansweetman</dc:creator>
    <dc:date>2015-06-29T21:29:41Z</dc:date>
    <item>
      <title>IMX6 Asynchronous Audmux/SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Asynchronous-Audmux-SSI/m-p/441329#M67811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having trouble getting SSI to work in asynchronous, 2 channel, network mode on the imx6 platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried using ssi as both a master and slave.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Master:&lt;/P&gt;&lt;P&gt;In the master configuration when i enable transmit I can see a correctly generated bit clk and frame sync present on the output of the audmux (port 4).&lt;/P&gt;&lt;P&gt;However&amp;nbsp; the same bit clk and frame sync is present on the receive lines even though the ssi controller, and both ports on the audmux are set to asynchronous.&lt;/P&gt;&lt;P&gt;There is no rx frame sync interrupt generated to the ssi controller however, and the txfs interrupt is fired only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i enable receive in this configuration instead, nothing comes out of the audmux on the receive or transmit lines, but the receive frame sync interrupt for the ssi controller is fired.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This lead me to believe the audmux was configured incorrectly, but other than disabling sync on that and setting the correct ports there doesn't to be anything else to do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR1: 00006000&lt;/P&gt;&lt;P&gt;PTCR1: 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR4: 00000000&lt;/P&gt;&lt;P&gt;PTCR4: 84210000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Slave:&lt;/P&gt;&lt;P&gt;I have been unable to get this to work at all, no matter the configuration that I use, synchronous or otherwise.&lt;/P&gt;&lt;P&gt;Unfortunately asynchronous slave is the ideal mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I have the audmux settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR1: 00006000&lt;/P&gt;&lt;P&gt;PTCR1: 9ce73000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR4: 00000000&lt;/P&gt;&lt;P&gt;PTCR4: 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I never get any form of frame sync interrupt no matter what I feed in.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2015 21:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Asynchronous-Audmux-SSI/m-p/441329#M67811</guid>
      <dc:creator>nathansweetman</dc:creator>
      <dc:date>2015-06-29T21:29:41Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Asynchronous Audmux/SSI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Asynchronous-Audmux-SSI/m-p/441330#M67812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nathan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding settings:&lt;/P&gt;&lt;P&gt;"PDCR1: 00006000&lt;/P&gt;&lt;P&gt;PTCR1: 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PDCR4: 00000000&lt;/P&gt;&lt;P&gt;PTCR4: 84210000"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe for asynchronous mode these should be changed to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PTCR4: 84210000 --&amp;gt; 84318000&lt;/P&gt;&lt;P&gt;RFSEL[3:0]=1000 Selects RXFS from port1.&lt;/P&gt;&lt;P&gt;RCSEL[3:0]=1000 Selects RXC&amp;nbsp; from port1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also for master/slave examples one can look at SDK audio examples,&lt;/P&gt;&lt;P&gt;where sgtl5000 is working as master, wm8262 as slave&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;i.MX 6Series Platform SDK&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2015 15:45:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Asynchronous-Audmux-SSI/m-p/441330#M67812</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-01T15:45:04Z</dc:date>
    </item>
  </channel>
</rss>