<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi'm facing problem with using yocto for fslimage bitbake.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-m-facing-problem-with-using-yocto-for-fslimage-bitbake/m-p/441294#M67800</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when i use yocto for making linux image, the system shows:&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_xor_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_sub_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_add_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_bool_compare_and_swap_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_or_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_and_4'&lt;/P&gt;&lt;P&gt;| collect2: ld returned 1 exit status&lt;/P&gt;&lt;P&gt;| make[4]: *** [gtester] Error 1&lt;/P&gt;&lt;P&gt;| make[4]: Leaving directory `/home/zhd/fsl-arm-yocto-bsp/build/tmp/work/i686-linux/glib-2.0-native/1_2.36.4-r0/build/glib'&lt;/P&gt;&lt;P&gt;| make[3]: *** [all-recursive] Error 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i 've searched the solution on the internet. they said it was caused because of my gcc version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but i find :&lt;/P&gt;&lt;P&gt;[root@localhost tmp]# yum install gcc&lt;/P&gt;&lt;P&gt;Loaded plugins: fastestmirror&lt;/P&gt;&lt;P&gt;Repository base is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository update is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository addons is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository extras is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository centosplus is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository contrib is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository testing is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Loading mirror speeds from cached hostfile&lt;/P&gt;&lt;P&gt; * epel: mirror01.idc.hinet.net&lt;/P&gt;&lt;P&gt;Setting up Install Process&lt;/P&gt;&lt;P&gt;Package gcc-4.1.2-55.el5.i386 already installed and latest version&lt;/P&gt;&lt;P&gt;Nothing to do&lt;/P&gt;&lt;P&gt;[root@localhost tmp]# &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so i think it's not because of my gcc version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;who can help me?&lt;/P&gt;&lt;P&gt;thanks a lot!&lt;/P&gt;&lt;P&gt;zhong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Jul 2015 02:54:35 GMT</pubDate>
    <dc:creator>dsfaf</dc:creator>
    <dc:date>2015-07-24T02:54:35Z</dc:date>
    <item>
      <title>i'm facing problem with using yocto for fslimage bitbake.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-m-facing-problem-with-using-yocto-for-fslimage-bitbake/m-p/441294#M67800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;when i use yocto for making linux image, the system shows:&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_xor_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_sub_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_add_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_bool_compare_and_swap_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_or_4'&lt;/P&gt;&lt;P&gt;| ./.libs/libglib-2.0.so: undefined reference to `__sync_fetch_and_and_4'&lt;/P&gt;&lt;P&gt;| collect2: ld returned 1 exit status&lt;/P&gt;&lt;P&gt;| make[4]: *** [gtester] Error 1&lt;/P&gt;&lt;P&gt;| make[4]: Leaving directory `/home/zhd/fsl-arm-yocto-bsp/build/tmp/work/i686-linux/glib-2.0-native/1_2.36.4-r0/build/glib'&lt;/P&gt;&lt;P&gt;| make[3]: *** [all-recursive] Error 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i 've searched the solution on the internet. they said it was caused because of my gcc version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but i find :&lt;/P&gt;&lt;P&gt;[root@localhost tmp]# yum install gcc&lt;/P&gt;&lt;P&gt;Loaded plugins: fastestmirror&lt;/P&gt;&lt;P&gt;Repository base is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository update is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository addons is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository extras is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository centosplus is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository contrib is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Repository testing is listed more than once in the configuration&lt;/P&gt;&lt;P&gt;Loading mirror speeds from cached hostfile&lt;/P&gt;&lt;P&gt; * epel: mirror01.idc.hinet.net&lt;/P&gt;&lt;P&gt;Setting up Install Process&lt;/P&gt;&lt;P&gt;Package gcc-4.1.2-55.el5.i386 already installed and latest version&lt;/P&gt;&lt;P&gt;Nothing to do&lt;/P&gt;&lt;P&gt;[root@localhost tmp]# &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so i think it's not because of my gcc version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;who can help me?&lt;/P&gt;&lt;P&gt;thanks a lot!&lt;/P&gt;&lt;P&gt;zhong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jul 2015 02:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-m-facing-problem-with-using-yocto-for-fslimage-bitbake/m-p/441294#M67800</guid>
      <dc:creator>dsfaf</dc:creator>
      <dc:date>2015-07-24T02:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: i'm facing problem with using yocto for fslimage bitbake.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-m-facing-problem-with-using-yocto-for-fslimage-bitbake/m-p/441295#M67801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Zhong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Would you please provide more details on your setup? Are you using the FSL BSP Release or the FSl Community BSP and for which board are you building? &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 20:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-m-facing-problem-with-using-yocto-for-fslimage-bitbake/m-p/441295#M67801</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-07-28T20:24:50Z</dc:date>
    </item>
  </channel>
</rss>