<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: vpu encoding/decoding parallely</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440601#M67650</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi GAUTAM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these figures are given for vpu standalone performance, that is without&lt;/P&gt;&lt;P&gt;additional applications (which may consume bandwidth) like rtp network,&lt;/P&gt;&lt;P&gt;please try with unit-test (imx-test) mxc_vpu_test&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/" title="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/"&gt;Index of /buildsources/i/imx-test/imx-test-3.14.28-1.0.0&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Jul 2015 10:40:51 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-07-27T10:40:51Z</dc:date>
    <item>
      <title>vpu encoding/decoding parallely</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440598#M67647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to encode camera buffers to H264 and stream the rtp packets and at same time i am recieving the H264 rtp packets and decoding it. I am using VPU through openmax layer for encoding and decoding . &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Stream is 720P and at 15 FPS it works fine, but at 25fps i see decoding becomes slow. And CPU usage becomes 80-90% .&amp;nbsp; As per documents VPU is capable of decoding 60 FPS &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions where to look into the issue. Does imx6 capable of 720P video conferencing ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 09:31:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440598#M67647</guid>
      <dc:creator>gautammanam</dc:creator>
      <dc:date>2015-07-23T09:31:36Z</dc:date>
    </item>
    <item>
      <title>Re: vpu encoding/decoding parallely</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440599#M67648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi GAUTAM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at presentation below p.6 it shows multistream performance:&lt;/P&gt;&lt;P&gt;2 simultaneous instances of 720p@30fps encode/decode, so seems for&lt;/P&gt;&lt;P&gt;encode+decode more realistic is 30fps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-95595"&gt;Q&amp;amp;amp;A: MX6 VPU H.264 Dual Stream Encode Limits&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For increasing vpu performance one can increase vpu frequency up to 352MHz,&lt;/P&gt;&lt;P&gt;Disable DFVS&lt;/P&gt;&lt;P&gt;echo performance &amp;gt; sys/devices/system/cpu/cpu0/cpufreq/scaling_governor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;some suggestions can found below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-93788"&gt;GStreamer i.MX6 Multi-Overlay&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for testing it is recommended to use imx-test/ mxc_vpu_test, included in BSP:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.14.28_1.0.0_iMX6QDLS_BUNDLE&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/" rel="nofollow"&gt;http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 10:43:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440599#M67648</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-23T10:43:33Z</dc:date>
    </item>
    <item>
      <title>Re: vpu encoding/decoding parallely</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440600#M67649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;When doing encoding/decoding simultaneously, i am getting around 30fps total for 720P H264 encode+decode. [15pfs for decoding and 15 fps for encoding] .&lt;/P&gt;&lt;P&gt;This is way less when compared to the above mentioned document. I can see i am getting enough rtp packets from network, but vpu decoder is slow in decoding&amp;nbsp; .And i am using VPU through fsl_imx_omx layer.&amp;nbsp; I am not sure if i am missing some thing. Can you suggest any VPU settings that i am missing. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IMX6Q sabre-Lite board&lt;/P&gt;&lt;P&gt;kernel 3.0.35&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2015 10:20:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440600#M67649</guid>
      <dc:creator>gautammanam</dc:creator>
      <dc:date>2015-07-27T10:20:24Z</dc:date>
    </item>
    <item>
      <title>Re: vpu encoding/decoding parallely</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440601#M67650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi GAUTAM&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;these figures are given for vpu standalone performance, that is without&lt;/P&gt;&lt;P&gt;additional applications (which may consume bandwidth) like rtp network,&lt;/P&gt;&lt;P&gt;please try with unit-test (imx-test) mxc_vpu_test&lt;/P&gt;&lt;P&gt;&lt;A href="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/" title="http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/"&gt;Index of /buildsources/i/imx-test/imx-test-3.14.28-1.0.0&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jul 2015 10:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpu-encoding-decoding-parallely/m-p/440601#M67650</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-27T10:40:51Z</dc:date>
    </item>
  </channel>
</rss>