<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SDIO voltage levels</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-voltage-levels/m-p/440581#M67643</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; The i.MX6 SL has two voltage suppliers : NVCC33_IO and NVCC18_IO.&lt;/P&gt;&lt;P&gt;The bit LVE in corresponding Pad Control Register defines what voltage will be&lt;/P&gt;&lt;P&gt;applied to the pin. Default value VLE=0 means 3.3V. &lt;/P&gt;&lt;P&gt;&amp;nbsp; The i.MX6 SL has special recommendations, when using so called low voltage&lt;/P&gt;&lt;P&gt;design, in particular it relates to 1.8V SD cards. Please refer to section 7.2.4 (Power-up&lt;/P&gt;&lt;P&gt;sequence in low voltage system design) of the “Hardware Development Guide for i.MX&lt;/P&gt;&lt;P&gt;6SoloLite - User Guide”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The i.MX6 D/Q/S/DL do not have ability to switch SD voltage internally.&lt;/P&gt;&lt;P&gt;An external scheme (power voltage switch or level translator) should be used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 May 2015 05:14:42 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-05-18T05:14:42Z</dc:date>
    <item>
      <title>SDIO voltage levels</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-voltage-levels/m-p/440580#M67642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we connect 1.8V device which communicates over SDIO directly to imx6 SDIO pins ? Or should we have level translator from 1.8V to 3.3V before connecting it to the imx6 SDIO pins&lt;/P&gt;&lt;P&gt;?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2015 04:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-voltage-levels/m-p/440580#M67642</guid>
      <dc:creator>jeevanmahadevu</dc:creator>
      <dc:date>2015-05-18T04:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: SDIO voltage levels</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SDIO-voltage-levels/m-p/440581#M67643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; The i.MX6 SL has two voltage suppliers : NVCC33_IO and NVCC18_IO.&lt;/P&gt;&lt;P&gt;The bit LVE in corresponding Pad Control Register defines what voltage will be&lt;/P&gt;&lt;P&gt;applied to the pin. Default value VLE=0 means 3.3V. &lt;/P&gt;&lt;P&gt;&amp;nbsp; The i.MX6 SL has special recommendations, when using so called low voltage&lt;/P&gt;&lt;P&gt;design, in particular it relates to 1.8V SD cards. Please refer to section 7.2.4 (Power-up&lt;/P&gt;&lt;P&gt;sequence in low voltage system design) of the “Hardware Development Guide for i.MX&lt;/P&gt;&lt;P&gt;6SoloLite - User Guide”&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; The i.MX6 D/Q/S/DL do not have ability to switch SD voltage internally.&lt;/P&gt;&lt;P&gt;An external scheme (power voltage switch or level translator) should be used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2015 05:14:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SDIO-voltage-levels/m-p/440581#M67643</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-05-18T05:14:42Z</dc:date>
    </item>
  </channel>
</rss>