<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Run boot.img from usb in u-boot time in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Run-boot-img-from-usb-in-u-boot-time/m-p/440363#M67588</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kulbhushan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please note that there are two Linux releases: official Freescale BSPs (which we [TIC] support) and Community BSPs (which we do not support, it is supported through Community or Yocto mailing list:&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://lists.yoctoproject.org/listinfo/meta-freescale" rel="nofollow"&gt;https://lists.yoctoproject.org/listinfo/meta-freescale&lt;/A&gt;&lt;SPAN&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Differences are described on below link&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://freescale.github.io/doc/release-notes/1.8/" rel="nofollow"&gt;http://freescale.github.io/doc/release-notes/1.8/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems uboot from Community BSPs releases supports USB in U-Boot. You could post your question on Yocto mailing list for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also refer to the following threads, which discus similar issues:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/376236"&gt;https://community.freescale.com/thread/376236&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/311585"&gt;https://community.freescale.com/thread/311585&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Oct 2015 18:44:03 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2015-10-30T18:44:03Z</dc:date>
    <item>
      <title>Run boot.img from usb in u-boot time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Run-boot-img-from-usb-in-u-boot-time/m-p/440362#M67587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using IMX6 sabre solo based board and I want to load boot.img form usb when i am at u-boot prompt.&lt;/P&gt;&lt;P&gt;what to do for load boot.img at u-boot prompt where boot.img is in usb?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kulbhushan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 13:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Run-boot-img-from-usb-in-u-boot-time/m-p/440362#M67587</guid>
      <dc:creator>kulbhushankashy</dc:creator>
      <dc:date>2015-10-29T13:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: Run boot.img from usb in u-boot time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Run-boot-img-from-usb-in-u-boot-time/m-p/440363#M67588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kulbhushan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please note that there are two Linux releases: official Freescale BSPs (which we [TIC] support) and Community BSPs (which we do not support, it is supported through Community or Yocto mailing list:&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://lists.yoctoproject.org/listinfo/meta-freescale" rel="nofollow"&gt;https://lists.yoctoproject.org/listinfo/meta-freescale&lt;/A&gt;&lt;SPAN&gt;).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Differences are described on below link&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://freescale.github.io/doc/release-notes/1.8/" rel="nofollow"&gt;http://freescale.github.io/doc/release-notes/1.8/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems uboot from Community BSPs releases supports USB in U-Boot. You could post your question on Yocto mailing list for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could also refer to the following threads, which discus similar issues:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/376236"&gt;https://community.freescale.com/thread/376236&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/311585"&gt;https://community.freescale.com/thread/311585&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 18:44:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Run-boot-img-from-usb-in-u-boot-time/m-p/440363#M67588</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2015-10-30T18:44:03Z</dc:date>
    </item>
  </channel>
</rss>