<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCSI 16bits on imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/CSI-16bits-on-imx6/m-p/440222#M67566</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this remaining question of capturing 16 bits yuv with external hsync/vsync ( IOMUX = D19~D12=Y, D11~D4=U/V,&amp;nbsp; PCLK+HSYNC+VSYNC),&lt;/P&gt;&lt;P&gt;(so in the case where bt1120 is not used but gated mode only).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;in &lt;/SPAN&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="357062" data-objecttype="2" href="https://community.freescale.com/message/357062#357062"&gt;https://community.freescale.com/message/357062#357062&lt;/A&gt;&lt;SPAN&gt;, Rogero Pimentel said in 2013 that "current Freescale Linux BSP doesn't support 16-bit input through CS"I.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is something new about that ? Is this configuration possible at the end ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jul 2015 09:12:50 GMT</pubDate>
    <dc:creator>christophe</dc:creator>
    <dc:date>2015-07-23T09:12:50Z</dc:date>
    <item>
      <title>CSI 16bits on imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-16bits-on-imx6/m-p/440222#M67566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For this remaining question of capturing 16 bits yuv with external hsync/vsync ( IOMUX = D19~D12=Y, D11~D4=U/V,&amp;nbsp; PCLK+HSYNC+VSYNC),&lt;/P&gt;&lt;P&gt;(so in the case where bt1120 is not used but gated mode only).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;in &lt;/SPAN&gt;&lt;A class="jive-link-message-small" data-containerid="2004" data-containertype="14" data-objectid="357062" data-objecttype="2" href="https://community.freescale.com/message/357062#357062"&gt;https://community.freescale.com/message/357062#357062&lt;/A&gt;&lt;SPAN&gt;, Rogero Pimentel said in 2013 that "current Freescale Linux BSP doesn't support 16-bit input through CS"I.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is something new about that ? Is this configuration possible at the end ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Christophe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 09:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-16bits-on-imx6/m-p/440222#M67566</guid>
      <dc:creator>christophe</dc:creator>
      <dc:date>2015-07-23T09:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: CSI 16bits on imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/CSI-16bits-on-imx6/m-p/440223#M67567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;pls refer to the link as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-97981"&gt;How to Support RGB565 Gated Mode Input to i.MX6 CSI&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jul 2015 08:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/CSI-16bits-on-imx6/m-p/440223#M67567</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2015-07-28T08:27:10Z</dc:date>
    </item>
  </channel>
</rss>