<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: External Memory Device Selection for i.MX535 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176573#M6750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark, thanks a lot for the info.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jul 2012 04:35:07 GMT</pubDate>
    <dc:creator>SrideviK</dc:creator>
    <dc:date>2012-07-25T04:35:07Z</dc:date>
    <item>
      <title>External Memory Device Selection for i.MX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176569#M6746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are developing a design based on i.MX535 processor (P/N MCIMX535DVV1C).&lt;/P&gt;&lt;P&gt;1. DRAM requirement - 512MB&lt;BR /&gt;We are planning to use LPDDR2 SDRAM,512MB(128Mx32) devices as given below:&lt;BR /&gt;(K4P4G324EC-AGC1 from SAMSUNG /&lt;BR /&gt;H9TKNNN4GDMPLR-NDM from HYNIX)&lt;/P&gt;&lt;P&gt;2. Flash requirement - 4GB&lt;BR /&gt;We are planning to use eMMC4.4.1 version Flash,4GB,153Pin devices as given below:&lt;BR /&gt;(KLM4G1FE3B-B001003 from SAMSUNG/&lt;BR /&gt;H26M31001FPR from HYNIX/&lt;BR /&gt;MTFC4GMTEA-1F WT from MICRON)&lt;/P&gt;&lt;P&gt;Pls advice whether the chosen parts are compatible for interface with i.MX535.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jul 2012 07:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176569#M6746</guid>
      <dc:creator>SrideviK</dc:creator>
      <dc:date>2012-07-22T07:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: External Memory Device Selection for i.MX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176570#M6747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale has used Hynix H5PS2G83AFR and Elpida EDB4032B1PB-8D-F LPDDR2 on i.MX53 family validation boards. But there is no reason why the above LPDD2 memory would not work. The Hynix H5P is a POP package. Your biggest choice will be to decide what footprint to use. The Samsung part you listed is also a POP package. Since footprints are controlled by the standards and it looks like you want to go with a POP package, I think you would be safe with either SAMSUNG/HYNIX. You can always easily substitute another if you run into problems. (But I don't think you will.)&lt;/P&gt;&lt;P&gt;The eMMC Flash that Freescale used on i.MX53 family validation boards is SanDisk SDIN5C2-8G. Again, the footprints are standard controlled and the above SAMSUNG/HYNIX/MICRON&amp;nbsp;eMMC managed flash should work&amp;nbsp;fine with the i.MX535 processor. eMMC is just an embedded MMC card.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jul 2012 16:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176570#M6747</guid>
      <dc:creator>TheAdmiral</dc:creator>
      <dc:date>2012-07-23T16:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: External Memory Device Selection for i.MX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176571#M6748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark for the clarification.&lt;/P&gt;&lt;P&gt;Is there any i.MX535 reference design with LPDDR2 &amp;amp; eMMC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2012 04:34:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176571#M6748</guid>
      <dc:creator>SrideviK</dc:creator>
      <dc:date>2012-07-24T04:34:27Z</dc:date>
    </item>
    <item>
      <title>Re: External Memory Device Selection for i.MX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176572#M6749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For eMMC, check out the i.MX53 SABRE Tablet schematics at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABRETAB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABRETAB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For LPDDR2, the i.MX50EVK was designed with LPDDR2. The i.MX508 chip is a member of the i.MX53 family, although it does not have the same footprint and is designed specifically for e-readers. This is the only publically avaiable design with the LPDDR2, but it is available only on the Freescale Customer Extranet site. If you would like access to this site, contact a local Freescale FAE. In reality, all DRAM is pretty easy to hook up. It is the physical layout that usually causes problems. Having said that, LPDDR2 on i.MX 6 is a little tricky because several pin functions were swizzled (swapped). But this does not apply to the i.MX53 processor.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;CITE&gt;Sridevi Kandaswamy said:&lt;/CITE&gt;&lt;/P&gt;&lt;BLOCKQUOTE cite="http://imxcommunity.org/forum/topics/external-memory-device-selection-for-i-mx535?groupUrl=imx53hardwaredesign&amp;amp;commentId=4103961%3AComment%3A76632&amp;amp;xg_source=msg_com_gr_forum#4103961Comment76632"&gt;&lt;DIV&gt;&lt;DIV class="xg_user_generated"&gt;&lt;P&gt;Thanks Mark for the clarification.&lt;/P&gt;&lt;P&gt;Is there any i.MX535 reference design with LPDDR2 &amp;amp; eMMC?&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2012 19:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176572#M6749</guid>
      <dc:creator>TheAdmiral</dc:creator>
      <dc:date>2012-07-24T19:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: External Memory Device Selection for i.MX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176573#M6750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mark, thanks a lot for the info.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2012 04:35:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176573#M6750</guid>
      <dc:creator>SrideviK</dc:creator>
      <dc:date>2012-07-25T04:35:07Z</dc:date>
    </item>
    <item>
      <title>Re: External Memory Device Selection for i.MX535</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176574#M6751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nothing to say,Only Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 09:01:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Memory-Device-Selection-for-i-MX535/m-p/176574#M6751</guid>
      <dc:creator>seganictech</dc:creator>
      <dc:date>2012-10-24T09:01:44Z</dc:date>
    </item>
  </channel>
</rss>