<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックi.MX6 eMMCv4.41 fast boot support?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439253#M67421</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In iMX6QD RM it says &lt;/P&gt;&lt;P&gt;"Fully compliant with MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41" and&lt;/P&gt;&lt;P&gt;also it says in boot section :&lt;/P&gt;&lt;P&gt;Boot code supports following standards.&lt;/P&gt;&lt;P&gt;• MMCv4.4 or less&lt;/P&gt;&lt;P&gt;• eMMCv4.4 or less&lt;/P&gt;&lt;P&gt;• SDv2.0 or less&lt;/P&gt;&lt;P&gt;• eSDv2.10 rev-0.9, with or without FAST_BOOT.&lt;/P&gt;&lt;P&gt;• SDXCv3.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two different statements above made me confused. The question is can i use eMMCv4.41 for fast boot mode of i.mx6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 17 May 2015 06:30:09 GMT</pubDate>
    <dc:creator>mehmetertugafsi</dc:creator>
    <dc:date>2015-05-17T06:30:09Z</dc:date>
    <item>
      <title>i.MX6 eMMCv4.41 fast boot support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439253#M67421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In iMX6QD RM it says &lt;/P&gt;&lt;P&gt;"Fully compliant with MMC command/response sets and Physical Layer as defined in the Multimedia Card System Specification, v4.2/4.3/4.4/4.41" and&lt;/P&gt;&lt;P&gt;also it says in boot section :&lt;/P&gt;&lt;P&gt;Boot code supports following standards.&lt;/P&gt;&lt;P&gt;• MMCv4.4 or less&lt;/P&gt;&lt;P&gt;• eMMCv4.4 or less&lt;/P&gt;&lt;P&gt;• SDv2.0 or less&lt;/P&gt;&lt;P&gt;• eSDv2.10 rev-0.9, with or without FAST_BOOT.&lt;/P&gt;&lt;P&gt;• SDXCv3.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Two different statements above made me confused. The question is can i use eMMCv4.41 for fast boot mode of i.mx6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 May 2015 06:30:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439253#M67421</guid>
      <dc:creator>mehmetertugafsi</dc:creator>
      <dc:date>2015-05-17T06:30:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 eMMCv4.41 fast boot support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439254#M67422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; The i.MX6 supports fast boot, as it is stated in section 67.4.9 (MMC fast boot)&lt;/P&gt;&lt;P&gt;of the i.MX6 DQ Reference Manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2015 21:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439254#M67422</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-05-19T21:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 eMMCv4.41 fast boot support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439255#M67423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, it is apparent that it supports MMC fast boot but the question is whether e.MMC version 4.41 is supported for fast boot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2015 18:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439255#M67423</guid>
      <dc:creator>mehmetertugafsi</dc:creator>
      <dc:date>2015-05-20T18:00:20Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 eMMCv4.41 fast boot support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439256#M67424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Yes, the boot ROM supports eMMC version 4.41 for fast boot.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;(ref. SR #&lt;A style="color: #51626f; font-family: 'Helvetica Neue', Helvetica, Arial, sans-serif; font-size: 11px; font-style: normal; font-weight: normal; text-align: start; text-indent: 0px;"&gt;&lt;SPAN align="left" style="color: #017bba;"&gt;&lt;STRONG&gt;1-987173450&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;SPAN style="color: #51626f; font-family: 'Helvetica Neue', Helvetica, Arial, sans-serif; font-size: 11px; font-style: normal; font-weight: normal; text-align: start; text-indent: 0px;"&gt;&lt;SPAN class="Apple-converted-space"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 06:02:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439256#M67424</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-05-26T06:02:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 eMMCv4.41 fast boot support?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439257#M67425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok thank you very much, i guess freescale should update the reference manuel and datasheet with the supoorted eMMC versions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2015 17:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-eMMCv4-41-fast-boot-support/m-p/439257#M67425</guid>
      <dc:creator>mehmetertugafsi</dc:creator>
      <dc:date>2015-05-26T17:43:15Z</dc:date>
    </item>
  </channel>
</rss>