<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx6 spi slave not receiving data</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438852#M67344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running mainline kernel 4.2.6 on hummingboard-gate (imx6solo).&lt;/P&gt;&lt;P&gt;Now I have one raspberryPI as SPI master and the hummingboard as slave.&lt;/P&gt;&lt;P&gt;I connected SS/SCLK/MISO/MOSI, the waveform looks correct, however I never see data ready bit set in imx6's spi status register, or irq triggered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all four pins are setup in IOMUXC as in pinmux tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ECSPI2 registers:&lt;/P&gt;&lt;P&gt;ECSPI_CONREG=0x00700001&lt;/P&gt;&lt;P&gt;ECSPI_CONFIGREG=0x000f0000&lt;/P&gt;&lt;P&gt;ECSPI_INTREG=0x00000008&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CCM's ecspi2 clk is enabled, irq requested is 64&lt;/P&gt;&lt;P&gt;spi master is configured as CS active low, mode 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do I need to setup anything else?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Nov 2015 17:49:11 GMT</pubDate>
    <dc:creator>hongfengwang</dc:creator>
    <dc:date>2015-11-24T17:49:11Z</dc:date>
    <item>
      <title>imx6 spi slave not receiving data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438852#M67344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am running mainline kernel 4.2.6 on hummingboard-gate (imx6solo).&lt;/P&gt;&lt;P&gt;Now I have one raspberryPI as SPI master and the hummingboard as slave.&lt;/P&gt;&lt;P&gt;I connected SS/SCLK/MISO/MOSI, the waveform looks correct, however I never see data ready bit set in imx6's spi status register, or irq triggered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;all four pins are setup in IOMUXC as in pinmux tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ECSPI2 registers:&lt;/P&gt;&lt;P&gt;ECSPI_CONREG=0x00700001&lt;/P&gt;&lt;P&gt;ECSPI_CONFIGREG=0x000f0000&lt;/P&gt;&lt;P&gt;ECSPI_INTREG=0x00000008&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CCM's ecspi2 clk is enabled, irq requested is 64&lt;/P&gt;&lt;P&gt;spi master is configured as CS active low, mode 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do I need to setup anything else?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 17:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438852#M67344</guid>
      <dc:creator>hongfengwang</dc:creator>
      <dc:date>2015-11-24T17:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 spi slave not receiving data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438853#M67345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hongfeng&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can try patch&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://lkml.iu.edu/hypermail/linux/kernel/1509.3/01176.html" rel="nofollow"&gt;http://lkml.iu.edu/hypermail/linux/kernel/1509.3/01176.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;or port older kernel patch&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2004" data-containertype="14" data-objectid="97380" data-objecttype="102" href="https://community.freescale.com/docs/DOC-97380"&gt;https://community.freescale.com/docs/DOC-97380&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Nov 2015 04:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438853#M67345</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-25T04:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 spi slave not receiving data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438854#M67346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I applied the patches in &lt;/P&gt;&lt;P&gt;&lt;A href="http://lkml.iu.edu/hypermail/linux/kernel/1509.3/01176.html" title="http://lkml.iu.edu/hypermail/linux/kernel/1509.3/01176.html"&gt;Linux-Kernel Archive: [PATCH v2 8/8] spi: imx: Add support for SPI Slave mode for imx53 and imx6 chips&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the hummingboard is able to receive data from SPI.&lt;/P&gt;&lt;P&gt;thanks for the help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Dec 2015 22:07:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438854#M67346</guid>
      <dc:creator>hongfengwang</dc:creator>
      <dc:date>2015-12-01T22:07:03Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 spi slave not receiving data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438855#M67347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi igorpadykov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to apply this patch to linux-3.10 for adding Spi slave mode ?&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" data-content-finding="Community" href="http://lkml.iu.edu/hypermail/linux/kernel/1509.3/01176.html" rel="nofollow"&gt;Linux-Kernel Archive: [PATCH v2 8/8] spi: imx: Add support for SPI Slave mode for imx53 and imx6 chips&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I applied below path to&amp;nbsp; linux-3.10 but, My imx6sx is not working as spi slave mode becaues spi rx isr doesn't get RX data.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-97380"&gt;i.MX6 ESPI slave mode support patch based on rel_imx_3.0.35_4.1.0&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you have any tip, please know to me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 12:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438855#M67347</guid>
      <dc:creator>moowonlee</dc:creator>
      <dc:date>2015-12-22T12:41:28Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 spi slave not receiving data</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438856#M67348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi hongfeng,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i use the same patch,but can't receive any data when imx6 as slave.would you like to tell me your register configs?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 02:37:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-spi-slave-not-receiving-data/m-p/438856#M67348</guid>
      <dc:creator>mingfang</dc:creator>
      <dc:date>2018-02-09T02:37:32Z</dc:date>
    </item>
  </channel>
</rss>