<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error in eMMC example iMX6 platform SDK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437818#M67143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this information, I will try to check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Apr 2015 07:51:48 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-04-24T07:51:48Z</dc:date>
    <item>
      <title>Error in eMMC example iMX6 platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437817#M67142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In mmc_read_esd in usdhc_mmc.c is an error in CMD8&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This line is correct:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;card_cmd_config(&amp;amp;cmd, CMD8, NO_ARG, READ, (1&amp;lt;&amp;lt;0)|(1&amp;lt;&amp;lt;2)|(1&amp;lt;&amp;lt;4), DATA_PRESENT, TRUE, TRUE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or host_data_read will never return.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 10:56:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437817#M67142</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2015-04-23T10:56:46Z</dc:date>
    </item>
    <item>
      <title>Re: Error in eMMC example iMX6 platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437818#M67143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this information, I will try to check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2015 07:51:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437818#M67143</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-24T07:51:48Z</dc:date>
    </item>
    <item>
      <title>Re: Error in eMMC example iMX6 platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437819#M67144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not possible to put the card into transfer mode.&lt;/P&gt;&lt;P&gt;card_enter_trans in usdhc.c CMD7 send fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;card_cmd_config(&amp;amp;cmd, CMD7, card_address, READ, (1&amp;lt;&amp;lt;0)|(1&amp;lt;&amp;lt;2)|(1&amp;lt;&amp;lt;4),//RESPONSE_48_CHECK_BUSY,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DATA_PRESENT_NONE, TRUE, TRUE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I ignore this, I can use card_data_read and card_data_write. Written data are saved, to weherever. Even after power down the data is still there, but whatever offset I choose, I get the same data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is a 4GB Toshiba eMMC chip on a Toradex Apalis board. Program is loaded over the serial bootloader, DCD and IVT from u-boot. Serial, GPIO and SPI works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2015 09:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437819#M67144</guid>
      <dc:creator>dirkschäfer</dc:creator>
      <dc:date>2015-04-24T09:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: Error in eMMC example iMX6 platform SDK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437820#M67145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Parameters of C-function card_cmd_config() are used to fill bit fields of Command Transfer Type &lt;BR /&gt;(uSDHCx_CMD_XFR_TYP)&amp;nbsp; register. Your pattern (1&amp;lt;&amp;lt;0)|(1&amp;lt;&amp;lt;2)|(1&amp;lt;&amp;lt;4) concerns the following &lt;BR /&gt;bit fields : &lt;/P&gt;&lt;P&gt;- CICEN (Command Index Check Enable) ;&lt;BR /&gt;- CCCEN (Command CRC Check Enable) ;&lt;BR /&gt;- RSPTYP[1:0] (Response Type Select).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The table below from the i.MX6 Reference Manual shows meaning of possible settings.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49351i8DDA191210575C6A/image-size/large?v=v2&amp;amp;px=999" title="response.jpg" alt="response.jpg" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last two parameters of C-function card_cmd_config() are used to configure&lt;/P&gt;&lt;P&gt;CICEN and CCCEN. Perhaps it would be better&amp;nbsp; to change them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2015 07:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Error-in-eMMC-example-iMX6-platform-SDK/m-p/437820#M67145</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-29T07:45:39Z</dc:date>
    </item>
  </channel>
</rss>