<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  same edid in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/same-edid/m-p/437658#M67112</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you to reply,I have solved the problem under your advice.thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Aug 2015 01:23:28 GMT</pubDate>
    <dc:creator>weisheng</dc:creator>
    <dc:date>2015-08-20T01:23:28Z</dc:date>
    <item>
      <title>same edid</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/same-edid/m-p/437656#M67110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have bought a new SABRE board for smart devices base on the I.MX6 series,but when I luanch the board,it post the message below on the screen：&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;egulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on&lt;/P&gt;&lt;P&gt;snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:01 UTC (1)&lt;/P&gt;&lt;P&gt;Freeing init memory: 244K&lt;/P&gt;&lt;P&gt;init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'&lt;/P&gt;&lt;P&gt;android_usb: already disabled&lt;/P&gt;&lt;P&gt;android_usb: already disabled&lt;/P&gt;&lt;P&gt;mtp_bind_config&lt;/P&gt;&lt;P&gt;root@android:/ # input: eCompass as /devices/virtual/input/input7&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: same edid&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: same edid&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: v4l2 capture: slave not found!&lt;/P&gt;&lt;P&gt;ERROR: HDMI is not ready!&lt;/P&gt;&lt;P&gt;asoc: can't open platform imx-hdmi-soc-audio.0&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: same edid&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: same edid&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: same edid&lt;/P&gt;&lt;P&gt;mxc_hdmi mxc_hdmi: same edid&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what's wrong with the board ,please help me out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 11:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/same-edid/m-p/437656#M67110</guid>
      <dc:creator>weisheng</dc:creator>
      <dc:date>2015-08-13T11:04:53Z</dc:date>
    </item>
    <item>
      <title>Re:  same edid</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/same-edid/m-p/437657#M67111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; Please check / change HDMI cable. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;If You are using HDMI/DVI converter :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp; It is required to add new 'allow_noncea=1' environment variable in the U-Boot &lt;BR /&gt; configuration and the arguments to set resolution to the kernel command line ; &lt;BR /&gt; as an example&amp;nbsp;&amp;nbsp; &lt;BR /&gt; 'video=mxcfb0:dev=hdmi,1280x1024M@60,if=RGB24'.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Also, the following may be helpful :&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;"HDMI Error on I.MX6Q SDB"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="jive-link-thread-small" data-containerid="2004" data-containertype="14" data-objectid="302840" data-objecttype="1" href="https://community.freescale.com/thread/302840"&gt;https://community.freescale.com/thread/302840&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 02:52:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/same-edid/m-p/437657#M67111</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-14T02:52:56Z</dc:date>
    </item>
    <item>
      <title>Re:  same edid</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/same-edid/m-p/437658#M67112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you to reply,I have solved the problem under your advice.thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2015 01:23:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/same-edid/m-p/437658#M67112</guid>
      <dc:creator>weisheng</dc:creator>
      <dc:date>2015-08-20T01:23:28Z</dc:date>
    </item>
  </channel>
</rss>