<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 mfgtool + secure boot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-secure-boot/m-p/437587#M67073</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are in the process of enabling high assurance boot on sabresd boards and in the process, we have updated the uboot for supporting hab and signed the uboot image for flashing on the device.&lt;/P&gt;&lt;P&gt;We used mfgtool for flashing and it worked fine until we updated and signed the uboot. After updating uboot, flashing by mfgtool, the board doesn't bootup either with signed uboot image nor the unsigned uboot image. Is there any configuration change that has to be done in the mfgtool to support uboot modifications or do we have to rebuild the mfgtool src for making the secure uboot to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Oct 2015 11:03:57 GMT</pubDate>
    <dc:creator>poonguzhalip</dc:creator>
    <dc:date>2015-10-28T11:03:57Z</dc:date>
    <item>
      <title>mfgtool + secure boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-secure-boot/m-p/437587#M67073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are in the process of enabling high assurance boot on sabresd boards and in the process, we have updated the uboot for supporting hab and signed the uboot image for flashing on the device.&lt;/P&gt;&lt;P&gt;We used mfgtool for flashing and it worked fine until we updated and signed the uboot. After updating uboot, flashing by mfgtool, the board doesn't bootup either with signed uboot image nor the unsigned uboot image. Is there any configuration change that has to be done in the mfgtool to support uboot modifications or do we have to rebuild the mfgtool src for making the secure uboot to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 11:03:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-secure-boot/m-p/437587#M67073</guid>
      <dc:creator>poonguzhalip</dc:creator>
      <dc:date>2015-10-28T11:03:57Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool + secure boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-secure-boot/m-p/437588#M67074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;uboot needs to built with mfg config and place it in OS Firmware folder &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 11:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-secure-boot/m-p/437588#M67074</guid>
      <dc:creator>poonguzhalip</dc:creator>
      <dc:date>2015-10-30T11:55:24Z</dc:date>
    </item>
    <item>
      <title>Re: mfgtool + secure boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/mfgtool-secure-boot/m-p/437589#M67075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can refer Application Note AN4581 "Secure Boot on i.MX50, i.MX53, and i.MX 6 Series using HABv4"&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4581.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 13:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/mfgtool-secure-boot/m-p/437589#M67075</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2015-10-30T13:01:38Z</dc:date>
    </item>
  </channel>
</rss>