<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIs there a way to program IMX6 internal RAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-a-way-to-program-IMX6-internal-RAM/m-p/437010#M66948</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just start to use IMX6.&lt;/P&gt;&lt;P&gt;I learned from IMX6DQRM that there is an internal RAM in IMX6 that have a provisioning program that allows to boot from boot device and program boot device.&lt;/P&gt;&lt;P&gt;I just wonder where can we download this source code and is there a way to program the IMX6 internal RAM?&lt;/P&gt;&lt;P&gt;The reason is that we want to change the saving location of Uboot in the boot device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ivy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2015 23:10:04 GMT</pubDate>
    <dc:creator>ivyliu</dc:creator>
    <dc:date>2015-07-22T23:10:04Z</dc:date>
    <item>
      <title>Is there a way to program IMX6 internal RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-a-way-to-program-IMX6-internal-RAM/m-p/437010#M66948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just start to use IMX6.&lt;/P&gt;&lt;P&gt;I learned from IMX6DQRM that there is an internal RAM in IMX6 that have a provisioning program that allows to boot from boot device and program boot device.&lt;/P&gt;&lt;P&gt;I just wonder where can we download this source code and is there a way to program the IMX6 internal RAM?&lt;/P&gt;&lt;P&gt;The reason is that we want to change the saving location of Uboot in the boot device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ivy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 23:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-a-way-to-program-IMX6-internal-RAM/m-p/437010#M66948</guid>
      <dc:creator>ivyliu</dc:creator>
      <dc:date>2015-07-22T23:10:04Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a way to program IMX6 internal RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-a-way-to-program-IMX6-internal-RAM/m-p/437011#M66949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; After reset the ARM core of i.MX6 begins execution starting from the on-chip boot ROM,&lt;/P&gt;&lt;P&gt;which contains code to provide boot for different devices. Please refer to Chapter 8&lt;/P&gt;&lt;P&gt;(System Boot) of the i.MX6 Reference Manual. Boot ROM source codes are not&lt;/P&gt;&lt;P&gt;provided and the boot ROM cannot be changed by users. In addition to boot ROM the i.MX6 &lt;/P&gt;&lt;P&gt;has internal RAM, which basically may be used by user's application. But please take into account , &lt;/P&gt;&lt;P&gt;that internal RAM is used by boot ROM during boot. Please refer to section 8.4.1 (Internal ROM /RAM &lt;/P&gt;&lt;P&gt;memory map).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 03:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-a-way-to-program-IMX6-internal-RAM/m-p/437011#M66949</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-07-23T03:15:21Z</dc:date>
    </item>
    <item>
      <title>Re: Is there a way to program IMX6 internal RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Is-there-a-way-to-program-IMX6-internal-RAM/m-p/437012#M66950</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I understand.&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ivy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 15:59:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Is-there-a-way-to-program-IMX6-internal-RAM/m-p/437012#M66950</guid>
      <dc:creator>ivyliu</dc:creator>
      <dc:date>2015-07-23T15:59:38Z</dc:date>
    </item>
  </channel>
</rss>