<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6 sabresd RTS in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sabresd-RTS/m-p/436522#M66840</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excuse me, TI am335x have register MCR, which can control RTS active low or inactive high. Does imx6 have similar register ? Because I think serial driver have full function of RS232, it must have some register to control RTS low or high, thank you. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2015 16:00:37 GMT</pubDate>
    <dc:creator>berniechen</dc:creator>
    <dc:date>2015-07-22T16:00:37Z</dc:date>
    <item>
      <title>imx6 sabresd RTS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sabresd-RTS/m-p/436522#M66840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excuse me, TI am335x have register MCR, which can control RTS active low or inactive high. Does imx6 have similar register ? Because I think serial driver have full function of RS232, it must have some register to control RTS low or high, thank you. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 16:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sabresd-RTS/m-p/436522#M66840</guid>
      <dc:creator>berniechen</dc:creator>
      <dc:date>2015-07-22T16:00:37Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sabresd RTS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sabresd-RTS/m-p/436523#M66841</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bernie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uart is described in Chapter 64&amp;nbsp;&amp;nbsp; &lt;A href="http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf?fasp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;IMX6DQRM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;there is no option to control RTS low or high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 01:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sabresd-RTS/m-p/436523#M66841</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-07-23T01:52:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sabresd RTS</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sabresd-RTS/m-p/436524#M66842</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But uart have full function, how do they implement RTS low and high?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 02:15:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sabresd-RTS/m-p/436524#M66842</guid>
      <dc:creator>berniechen</dc:creator>
      <dc:date>2015-07-23T02:15:03Z</dc:date>
    </item>
  </channel>
</rss>