<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question, i.MX28 LRADC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-LRADC/m-p/435941#M66750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about LRADC of i.MX28.&lt;/P&gt;&lt;P&gt;From the description in i.MX28 datasheet, the power source of LRADC seems to be VDDA. Right?&lt;/P&gt;&lt;P&gt;And the datasheet says that the maximum voltage of LDRADC is 1.85V.&lt;/P&gt;&lt;P&gt;(1)&lt;/P&gt;&lt;P&gt;Is it possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V?&lt;/P&gt;&lt;P&gt;(2)&lt;/P&gt;&lt;P&gt;The reference voltage, the internal Bandgap reference, for the ADC is always 1.85V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Aug 2015 03:10:39 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-08-13T03:10:39Z</dc:date>
    <item>
      <title>Question, i.MX28 LRADC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-LRADC/m-p/435941#M66750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about LRADC of i.MX28.&lt;/P&gt;&lt;P&gt;From the description in i.MX28 datasheet, the power source of LRADC seems to be VDDA. Right?&lt;/P&gt;&lt;P&gt;And the datasheet says that the maximum voltage of LDRADC is 1.85V.&lt;/P&gt;&lt;P&gt;(1)&lt;/P&gt;&lt;P&gt;Is it possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V?&lt;/P&gt;&lt;P&gt;(2)&lt;/P&gt;&lt;P&gt;The reference voltage, the internal Bandgap reference, for the ADC is always 1.85V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 03:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-LRADC/m-p/435941#M66750</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-08-13T03:10:39Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX28 LRADC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-LRADC/m-p/435942#M66751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. From the description in i.MX28 datasheet, the power source of LRADC seems to be VDDA. Right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. No, this is not right. The supply voltage for LRADC is fed directly from the Power Supply module, it is derived from either Battery or V4P2 voltage by a linear regulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. Is it possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. As told before, VDDA does not affect the LRADC operation. So, the answer is: yes, it is possible for LRADC to operate correctly for 1.85V input to LRADC, in the situation that VDDA is lower than 1.85V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. The reference voltage, the internal Bandgap reference, for the ADC is always 1.85V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Yes.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 08:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-LRADC/m-p/435942#M66751</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-08-13T08:42:45Z</dc:date>
    </item>
  </channel>
</rss>