<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question, i.MX6Q USB data transfer is wrong while playing video in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-data-transfer-is-wrong-while-playing-video/m-p/435412#M66636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about the issue of USB data transfer which my customer faces.&lt;/P&gt;&lt;P&gt;On the customer’s board, USB camera is connected to i.MX6Q. And they use Android4.0(based on your androidBSP) for OS.&lt;/P&gt;&lt;P&gt;They saw the camera data seemed to be corrupted or missing when i.MX6 was playing H.264 video at 60fps(the resolution was QVGA).&lt;/P&gt;&lt;P&gt;When the frame rate of playing video was 30fps, the USB camera’s data seemed to be OK.&lt;/P&gt;&lt;P&gt;This phenomenon of USB camera data is also seen when Hello-gl2, sample program included in NDK, is executed on i.MX6.&lt;/P&gt;&lt;P&gt;From the above, they believe the cause of this issue is related to the internal BUS load of i.MX6.&lt;/P&gt;&lt;P&gt;Do you have any ideas on the cause of this issue?&lt;/P&gt;&lt;P&gt;On the customer’s board, The USB camera data needs to be captured correctly even when the video is playing at 60fps simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Apr 2015 00:36:43 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-04-23T00:36:43Z</dc:date>
    <item>
      <title>Question, i.MX6Q USB data transfer is wrong while playing video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-data-transfer-is-wrong-while-playing-video/m-p/435412#M66636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about the issue of USB data transfer which my customer faces.&lt;/P&gt;&lt;P&gt;On the customer’s board, USB camera is connected to i.MX6Q. And they use Android4.0(based on your androidBSP) for OS.&lt;/P&gt;&lt;P&gt;They saw the camera data seemed to be corrupted or missing when i.MX6 was playing H.264 video at 60fps(the resolution was QVGA).&lt;/P&gt;&lt;P&gt;When the frame rate of playing video was 30fps, the USB camera’s data seemed to be OK.&lt;/P&gt;&lt;P&gt;This phenomenon of USB camera data is also seen when Hello-gl2, sample program included in NDK, is executed on i.MX6.&lt;/P&gt;&lt;P&gt;From the above, they believe the cause of this issue is related to the internal BUS load of i.MX6.&lt;/P&gt;&lt;P&gt;Do you have any ideas on the cause of this issue?&lt;/P&gt;&lt;P&gt;On the customer’s board, The USB camera data needs to be captured correctly even when the video is playing at 60fps simultaneously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 00:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-data-transfer-is-wrong-while-playing-video/m-p/435412#M66636</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-04-23T00:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX6Q USB data transfer is wrong while playing video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-data-transfer-is-wrong-while-playing-video/m-p/435413#M66637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Miyamoto,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; Your idea, that “the cause of this issue is related to the internal BUS load of i.MX6” is quite reasonable.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; If system / memory bus&amp;nbsp; load is high, because many modules, using DMA, are working simultaneously &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;(VPU, DMA, IPU, GPU, SD as system storage)&amp;nbsp; some data may be lost because of modules FIFO over-/under-load.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt; You may try the following in order to improve situation :&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;1) disable bus frequency feature. Take a look at section 17 (How do I enable or disable&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; the bus frequency feature?) of the “Android_Frequently_Asked_Questions.pdf” in Android &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; documentation.&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;2) to optimize memory usage. Please refer to&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;“Memory Management on i.MX6 Android”&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A _jive_internal="true" data-containerid="2004" data-containertype="14" data-objectid="93591" data-objecttype="102" href="https://community.nxp.com/docs/DOC-93591"&gt;https://community.freescale.com/docs/DOC-93591&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;The following material may be useful &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;“Memory Issue in i.MX5 Android”&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;lt; &lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&lt;A class="" href="https://community.freescale.com/servlet/JiveServlet/previewBody/"&gt;https://community.freescale.com/servlet/JiveServlet/previewBody/&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;93334-102-1-2448/iMX5%20Android%20GB%20Memory%20Usage%20and%20Optimization.pdf &amp;gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Have a great day,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Yuri&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Apr 2015 07:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX6Q-USB-data-transfer-is-wrong-while-playing-video/m-p/435413#M66637</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-04-24T07:56:35Z</dc:date>
    </item>
  </channel>
</rss>