<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: External RTC</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/External-RTC/m-p/435333#M66618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. How this can be corrected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Check the crystal tolerance first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. Will there be any issue in booting or timing on using external RTC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. No, there should be no any issue. You just have to slightly modify the software to load the value of the external RTC to the internal one each boot time.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Nov 2015 10:54:37 GMT</pubDate>
    <dc:creator>art</dc:creator>
    <dc:date>2015-11-26T10:54:37Z</dc:date>
    <item>
      <title>External RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-RTC/m-p/435332#M66617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using internal RTC with a crystal of 9pF load capacitance and two 16pF capacitors on i.MX6S processor. The clock is about 2 to 3 seconds lagging behind on every 2 days. How this can be corrected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are thinking to use external RTC, which will provide clock on I2C lines to processor. Will there be any issue in booting or timing on using external RTC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with regards&lt;/P&gt;&lt;P&gt;Lalit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 07:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-RTC/m-p/435332#M66617</guid>
      <dc:creator>lk22</dc:creator>
      <dc:date>2015-11-24T07:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: External RTC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-RTC/m-p/435333#M66618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Q. How this can be corrected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. Check the crystal tolerance first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q. Will there be any issue in booting or timing on using external RTC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A. No, there should be no any issue. You just have to slightly modify the software to load the value of the external RTC to the internal one each boot time.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Nov 2015 10:54:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-RTC/m-p/435333#M66618</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-11-26T10:54:37Z</dc:date>
    </item>
  </channel>
</rss>