<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PMIC GUI: Program and Verify Buttons not highlighted</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435110#M66575</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"&lt;SPAN style="color: #1f497d;"&gt;To do the program, after load the script, it needs to click the “Convert Script File” button on the bottom firstly, then you will the the “PROGRAM”&amp;nbsp; button will switch from gray to green. It is recommended to click “Verify After Programming” button at the same time.&lt;/SPAN&gt;" &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did that and the Program button never turned green.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are the Buck and Linear Supplies Panels showing configuration for both the PMIC soldered to the EVAL board AND the loose PMIC part I placed into the socket programmer board that is plugged into the EVAL board I2c header?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Aug 2015 13:16:50 GMT</pubDate>
    <dc:creator>michaelbazarov</dc:creator>
    <dc:date>2015-08-13T13:16:50Z</dc:date>
    <item>
      <title>PMIC GUI: Program and Verify Buttons not highlighted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435107#M66572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using GUI Rev 4 and the PMIC PF0100 Eval board along with the socket board to try and set OTP fuses on unprogrammed PMICs. I have the script for the configuration I want but the program and verify buttons are not clickable. I placed J17 jumpers accross pins 1 and 2 to allow OTP programming and ran my OTP script in the script editor. Pretty sure I burned the fuses on the embedded eval board PMIC but when I click "Blank device" it now says device programmed when before it said device blank. Is there a way to get the GUI to verify my configuration? Did i even program the new part i placed in the socket board or just the one on the eval board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 20:26:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435107#M66572</guid>
      <dc:creator>michaelbazarov</dc:creator>
      <dc:date>2015-08-12T20:26:40Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC GUI: Program and Verify Buttons not highlighted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435108#M66573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mike,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&amp;nbsp;&amp;nbsp; It the part has already programmed, when the board connect to the GUI, Enable Target, the “Buck Supplies” and “Linear Supplies”&amp;nbsp; panel will show the fuses information about the part, you can check if this is what you want.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;To do the program, after load the script, it needs to click the “Convert Script File” button on the bottom firstly, then you will the the “PROGRAM”&amp;nbsp; button will switch from gray to green. It is recommended to click “Verify After Programming” button at the same time.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt; Reards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 03:50:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435108#M66573</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2015-08-13T03:50:26Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC GUI: Program and Verify Buttons not highlighted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435109#M66574</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the Chapter 5 of the attached document.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 08:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435109#M66574</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-08-13T08:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC GUI: Program and Verify Buttons not highlighted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435110#M66575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"&lt;SPAN style="color: #1f497d;"&gt;To do the program, after load the script, it needs to click the “Convert Script File” button on the bottom firstly, then you will the the “PROGRAM”&amp;nbsp; button will switch from gray to green. It is recommended to click “Verify After Programming” button at the same time.&lt;/SPAN&gt;" &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did that and the Program button never turned green.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are the Buck and Linear Supplies Panels showing configuration for both the PMIC soldered to the EVAL board AND the loose PMIC part I placed into the socket programmer board that is plugged into the EVAL board I2c header?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 13:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435110#M66575</guid>
      <dc:creator>michaelbazarov</dc:creator>
      <dc:date>2015-08-13T13:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC GUI: Program and Verify Buttons not highlighted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435111#M66576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What socket programmer board do you use? Please specify.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Artur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 08:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435111#M66576</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-08-14T08:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC GUI: Program and Verify Buttons not highlighted</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435112#M66577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;KITPF0100SKTEVBE&lt;/P&gt;&lt;P&gt;700-27867 Rev B&lt;/P&gt;&lt;P&gt;SCH-27867 Rev B&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Aug 2015 13:33:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-GUI-Program-and-Verify-Buttons-not-highlighted/m-p/435112#M66577</guid>
      <dc:creator>michaelbazarov</dc:creator>
      <dc:date>2015-08-17T13:33:25Z</dc:date>
    </item>
  </channel>
</rss>