<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 EIM Synchronous mode</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Synchronous-mode/m-p/434697#M66450</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a project that use IMX6D EIM interface to communicate with FPGA， I have configured the EIM timing as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. synchronous read/write mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. MUM = 1, DSZ = 001, that is Multiplexed Address/Data mode and Data width is 16 bit。&lt;/P&gt;&lt;P&gt;When I read or write the EIM interface, The FPGA side sampling the bus signal with chip scope. We found that the address is increased by four, for example:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00, 0x04, 0x08, 0x0C, 0x10, ......&lt;/P&gt;&lt;P&gt;That is confused, the data width is 16, address bus should increased by 2, why is 4? &lt;/P&gt;&lt;P&gt;anyone can help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Oct 2015 01:33:18 GMT</pubDate>
    <dc:creator>thouswave</dc:creator>
    <dc:date>2015-10-28T01:33:18Z</dc:date>
    <item>
      <title>EIM Synchronous mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Synchronous-mode/m-p/434697#M66450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a project that use IMX6D EIM interface to communicate with FPGA， I have configured the EIM timing as:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. synchronous read/write mode&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. MUM = 1, DSZ = 001, that is Multiplexed Address/Data mode and Data width is 16 bit。&lt;/P&gt;&lt;P&gt;When I read or write the EIM interface, The FPGA side sampling the bus signal with chip scope. We found that the address is increased by four, for example:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00, 0x04, 0x08, 0x0C, 0x10, ......&lt;/P&gt;&lt;P&gt;That is confused, the data width is 16, address bus should increased by 2, why is 4? &lt;/P&gt;&lt;P&gt;anyone can help me?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 01:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-Synchronous-mode/m-p/434697#M66450</guid>
      <dc:creator>thouswave</dc:creator>
      <dc:date>2015-10-28T01:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: EIM Synchronous mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/EIM-Synchronous-mode/m-p/434698#M66451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Start access address depends on ARM instruction used for it.&lt;/P&gt;&lt;P&gt;Say, LDR is for 32-bit data and address is aligned for 32-bit.&lt;/P&gt;&lt;P&gt;LDRH : for 16-bit data.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 03:08:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/EIM-Synchronous-mode/m-p/434698#M66451</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-28T03:08:06Z</dc:date>
    </item>
  </channel>
</rss>