<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: USB OTG ISSUE</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-ISSUE/m-p/434537#M66434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Vishnu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check VDD_VBUS_CAP voltage and&lt;/P&gt;&lt;P&gt;check 24MHz frequency, if it is not stable usb communnication fails.&lt;/P&gt;&lt;P&gt;For testing one can load uboot with jtag, then test usb:&lt;/P&gt;&lt;P&gt;usb start , fatls usb 0:1&lt;/P&gt;&lt;P&gt;From PC (preferably with XP OS) one can run MFG Tools and connect board&lt;/P&gt;&lt;P&gt;with usb cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Nov 2015 01:48:38 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-11-24T01:48:38Z</dc:date>
    <item>
      <title>USB OTG ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-ISSUE/m-p/434536#M66433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi There,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have done a imx6q based design and board bring up is going on.&lt;/P&gt;&lt;P&gt;All the power rails, clk, por are okay..(We followed our development board's power sequence which is working) but when we tried to connect OTG port to a computer it's not detecting it.&lt;/P&gt;&lt;P&gt;Board is not booted yet ..(no SD boot option provided)&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Vishnu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 09:57:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-ISSUE/m-p/434536#M66433</guid>
      <dc:creator>vishnuharihar</dc:creator>
      <dc:date>2015-11-23T09:57:15Z</dc:date>
    </item>
    <item>
      <title>Re: USB OTG ISSUE</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-ISSUE/m-p/434537#M66434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Vishnu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check VDD_VBUS_CAP voltage and&lt;/P&gt;&lt;P&gt;check 24MHz frequency, if it is not stable usb communnication fails.&lt;/P&gt;&lt;P&gt;For testing one can load uboot with jtag, then test usb:&lt;/P&gt;&lt;P&gt;usb start , fatls usb 0:1&lt;/P&gt;&lt;P&gt;From PC (preferably with XP OS) one can run MFG Tools and connect board&lt;/P&gt;&lt;P&gt;with usb cable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 01:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-OTG-ISSUE/m-p/434537#M66434</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-11-24T01:48:38Z</dc:date>
    </item>
  </channel>
</rss>