<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Failure compiling busybox with PAM support</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Failure-compiling-busybox-with-PAM-support/m-p/434392#M66391</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vicente,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using LTIB for this compilation? what version of BSP are you using?&amp;nbsp; Check the makefile of the BusyBox ( PAM)&amp;nbsp; in order to see the dependencies required or in the readme file what requirements of the Kernel or options need to be setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;saludos&lt;/P&gt;&lt;P&gt;Jaime&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Nov 2015 20:40:07 GMT</pubDate>
    <dc:creator>jamesbone</dc:creator>
    <dc:date>2015-11-05T20:40:07Z</dc:date>
    <item>
      <title>Failure compiling busybox with PAM support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-compiling-busybox-with-PAM-support/m-p/434391#M66390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using L2.6.31_09.12.01&lt;/P&gt;&lt;P&gt;I have selected support for PAM in busybox package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The result of the compilation of busybox package is like this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;pam_appl.h&amp;nbsp; No such file or directory&lt;/P&gt;&lt;P&gt;pam_misc.h: No such file or directory&lt;/P&gt;&lt;P&gt;and many other error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think i need to add another options or packages but i don´t know what options or packages to add&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anybody know what to do in that situation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Oct 2015 21:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-compiling-busybox-with-PAM-support/m-p/434391#M66390</guid>
      <dc:creator>josévicentesana</dc:creator>
      <dc:date>2015-10-27T21:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: Failure compiling busybox with PAM support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Failure-compiling-busybox-with-PAM-support/m-p/434392#M66391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vicente,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using LTIB for this compilation? what version of BSP are you using?&amp;nbsp; Check the makefile of the BusyBox ( PAM)&amp;nbsp; in order to see the dependencies required or in the readme file what requirements of the Kernel or options need to be setup.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;saludos&lt;/P&gt;&lt;P&gt;Jaime&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Nov 2015 20:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Failure-compiling-busybox-with-PAM-support/m-p/434392#M66391</guid>
      <dc:creator>jamesbone</dc:creator>
      <dc:date>2015-11-05T20:40:07Z</dc:date>
    </item>
  </channel>
</rss>