<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Eclipse Yocto Autotool Project Add Folder</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434299#M66377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am using Eclipse Yocto ADT plugin for application development.&lt;/P&gt;&lt;P&gt;I have created Yocto ADT Autotool project.&lt;/P&gt;&lt;P&gt;In the project i can use function of any file from "/opt/poky/1.8/sysroots/cortexa9hf-vpf-neon-poky-linux-gnueabi/user/include".&lt;/P&gt;&lt;P&gt;But i want to use files from other directory. so i add paths in "C/C++ General/Path and symbols/include directories".&lt;/P&gt;&lt;P&gt;Now function reference can be found by eclipse. I can also Jump to defination by F3.&lt;/P&gt;&lt;P&gt;But when i compile i get "fatal error: No file or directory"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So how to add other folder with no error? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Aug 2015 12:52:07 GMT</pubDate>
    <dc:creator>ritesh_panchal</dc:creator>
    <dc:date>2015-08-13T12:52:07Z</dc:date>
    <item>
      <title>Eclipse Yocto Autotool Project Add Folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434299#M66377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i am using Eclipse Yocto ADT plugin for application development.&lt;/P&gt;&lt;P&gt;I have created Yocto ADT Autotool project.&lt;/P&gt;&lt;P&gt;In the project i can use function of any file from "/opt/poky/1.8/sysroots/cortexa9hf-vpf-neon-poky-linux-gnueabi/user/include".&lt;/P&gt;&lt;P&gt;But i want to use files from other directory. so i add paths in "C/C++ General/Path and symbols/include directories".&lt;/P&gt;&lt;P&gt;Now function reference can be found by eclipse. I can also Jump to defination by F3.&lt;/P&gt;&lt;P&gt;But when i compile i get "fatal error: No file or directory"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So how to add other folder with no error? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Aug 2015 12:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434299#M66377</guid>
      <dc:creator>ritesh_panchal</dc:creator>
      <dc:date>2015-08-13T12:52:07Z</dc:date>
    </item>
    <item>
      <title>Re: Eclipse Yocto Autotool Project Add Folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434300#M66378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Verdana','sans-serif';"&gt;&amp;nbsp;&amp;nbsp; Looks like it is necessary to add include path in “C/C++ Build -&amp;gt;Settings -&amp;gt; ARM C compiler -&amp;gt; Includes”.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 09:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434300#M66378</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-14T09:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: Eclipse Yocto Autotool Project Add Folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434301#M66379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;In C/C++ Build -&amp;gt;Settings -&amp;gt; there is no option like ARM C compiler -&amp;gt; Includes. This is because i am using Eclipse Yocto ADT Autotool Project.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;Please see attached image.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot from 2015-08-14 15_00_47.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52519i4F3FB969150A6153/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2015-08-14 15_00_47.png" alt="Screenshot from 2015-08-14 15_00_47.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;If i create Executable ANSI C project ARM C Compiler options will appear.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;I am using Yocto ADT project because i don't need to add Cross compiler settings or environment variable. I am following the steps as per given in the Yocto Developer manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;If i create Executable Project i need to add all Environment variable.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;I have added SDK folder path as per snapshot below.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot from 2015-08-14 15_05_40.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52548i398318E0DE27CD42/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2015-08-14 15_05_40.png" alt="Screenshot from 2015-08-14 15_05_40.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Verdana, sans-serif;"&gt;So whats the reason i am getting No files or directory error.?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 09:37:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434301#M66379</guid>
      <dc:creator>ritesh_panchal</dc:creator>
      <dc:date>2015-08-14T09:37:14Z</dc:date>
    </item>
    <item>
      <title>Re: Eclipse Yocto Autotool Project Add Folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434302#M66380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following may be useful :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-106613"&gt;Yocto Application Development Using Eclipse IDE&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2015 04:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Eclipse-Yocto-Autotool-Project-Add-Folder/m-p/434302#M66380</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-26T04:32:49Z</dc:date>
    </item>
  </channel>
</rss>