<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: imx6 sata cdrom driver issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434258#M66364</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Experiments / findings from my co-worker Kevin....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the debug patch I wrote that Jon posted earlier I can see that the&lt;/P&gt;&lt;P&gt;response to the ATAPI 0x4A command (Get Event Status Notification)&lt;/P&gt;&lt;P&gt;during initial boot is always random. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 2.237783] CDB rbuf: [4a 01 00 00 10 00 00 00 08]&lt;/P&gt;&lt;P&gt;[ 2.237789] CDB rbuf: 00000000: 7e 31 f7 fd ff f5 7d fd&lt;/P&gt;&lt;P&gt;~1....}.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Running the same test on an iMX53 EVK board the response is always:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[ 2.452303] CDB rbuf: [4a 01 00 00 10 00 00 00 08]&lt;/P&gt;&lt;P&gt;[ 2.452308] CDB rbuf: 00000000: 00 06 04 56 02 02 00 00&lt;/P&gt;&lt;P&gt;...V....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have rented a Lecroy STX-231 SATA protocol analyzer. Using this tool&lt;/P&gt;&lt;P&gt;I have verified that the response from the optical drive is always&lt;/P&gt;&lt;P&gt;correct in this case but for some reason the data is corrupt by the time&lt;/P&gt;&lt;P&gt;the debug code I added to atapi_qc_complete dumps the response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have added debug code to dump the AHCI command header and table before&lt;/P&gt;&lt;P&gt;issuing a command. I have not seen anything out of the ordinary here. I&lt;/P&gt;&lt;P&gt;also added debug code to dump the received FIS on an interrupt. I&lt;/P&gt;&lt;P&gt;haven't studied the received FIS extensively but I did not see anything&lt;/P&gt;&lt;P&gt;out of the ordinary here either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One thing I suspected and confirmed with the Lecroy analyzer is that the&lt;/P&gt;&lt;P&gt;response to the previous command during boot (ATAPI command 0x5A - Mode&lt;/P&gt;&lt;P&gt;Sense) is always 64 bytes even though the kernel is requesting 128&lt;/P&gt;&lt;P&gt;bytes. This exact behaviour is probably drive dependant. On a hunch I&lt;/P&gt;&lt;P&gt;modified the get_capabilities function in drivers/scsi/sr.c to only&lt;/P&gt;&lt;P&gt;request 64 bytes. With that change the response to the Get Event Status&lt;/P&gt;&lt;P&gt;Notification command during boot is always valid. Although running&lt;/P&gt;&lt;P&gt;cdparanoia or trying to keep using the system in other ways still&lt;/P&gt;&lt;P&gt;results in issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using the Lecroy analyzer I found some other commands where cdparanoia&lt;/P&gt;&lt;P&gt;requests lengths longer than the drive responds with. Comparing the&lt;/P&gt;&lt;P&gt;debug dumps in the kernel to the data captured by the analyzer I can see&lt;/P&gt;&lt;P&gt;problems always start after this happens.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To try and characterize this further I started messing around with the&lt;/P&gt;&lt;P&gt;request lengths. I noticed in the AHCI command header dumps I added&lt;/P&gt;&lt;P&gt;that many of the ATAPI commands have a second SG DMA buffer. I found the&lt;/P&gt;&lt;P&gt;second buffer is added when atapi_drain_needed returns true in&lt;/P&gt;&lt;P&gt;libata-scsi.c. I started hacking the DMA buffer sizes by manipulating&lt;/P&gt;&lt;P&gt;the lengths written to the AHCI command table in the ahci_fill_sg&lt;/P&gt;&lt;P&gt;function in libata.c. I also hacked atap_drain_needed to sometimes&lt;/P&gt;&lt;P&gt;return false to force only one DMA buffer for ATAPI commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I found is that if there are two DMA buffers and the response&lt;/P&gt;&lt;P&gt;length is less than the first buffer size then the response to the next&lt;/P&gt;&lt;P&gt;command is always corrupted. Every other scenario I tried worked okay.&lt;/P&gt;&lt;P&gt;Filling the first buffer and under, over or exactly using the second&lt;/P&gt;&lt;P&gt;buffer does not trigger the issue. If there is only one buffer under,&lt;/P&gt;&lt;P&gt;over or exactly using the one buffer does not trigger the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One other thing I noticed is that if the response under runs the first&lt;/P&gt;&lt;P&gt;buffer and the second ATAPI drain buffer is smaller than the next&lt;/P&gt;&lt;P&gt;command response then the response to the next command is missing the&lt;/P&gt;&lt;P&gt;begging of the response equal to the length of the second buffer from&lt;/P&gt;&lt;P&gt;the previous command. I decided to add some debug code to print out the&lt;/P&gt;&lt;P&gt;DMA buffer used for the previous command. What I found is that the&lt;/P&gt;&lt;P&gt;missing part of the response is written to the DMA buffer from the&lt;/P&gt;&lt;P&gt;previous command. This is very bad as that memory could be dynamically&lt;/P&gt;&lt;P&gt;allocated and subsequently freed and now in use by something else!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since overruns never seem to cause an issue in this setup I decided to&lt;/P&gt;&lt;P&gt;simply change the atap_drain_needed function to always return false.&lt;/P&gt;&lt;P&gt;With this change I can run cdparanoia successfully and rip audio tracks.&lt;/P&gt;&lt;P&gt;I can also add a port multiplier back to the setup and connect both an&lt;/P&gt;&lt;P&gt;HDD and the optical drive and experience no readily apparent issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it seems I have found a workaround for the most severe symptoms we&lt;/P&gt;&lt;P&gt;were experiencing. But this still leaves me with several questions and&lt;/P&gt;&lt;P&gt;concerns:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Is the root cause some obscure bug in the kernel I have not found&lt;/P&gt;&lt;P&gt;yet? Or is it a hardware bug in the iMX6 AHCI SATA host? Or maybe&lt;/P&gt;&lt;P&gt;something else silly we have been doing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. When cdparanoia is ripping the actual data it uses large reads which&lt;/P&gt;&lt;P&gt;use multiple SG DMA buffers. What happens if the response is short in&lt;/P&gt;&lt;P&gt;this case? My atapi_drain_needed hack won't help in this case.&lt;/P&gt;&lt;P&gt;cdparanoia could probably be modified to only do smaller reads that fit&lt;/P&gt;&lt;P&gt;in one page to avoid the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. Can the issue happen with non ATAPI commands? If for any reason an&lt;/P&gt;&lt;P&gt;ATA command to a HDD has a short response could all future commands (and&lt;/P&gt;&lt;P&gt;possibly even system memory) be corrupted similar to what I saw with&lt;/P&gt;&lt;P&gt;ATAPI commands? I wonder if the kernel could be easily modified to limit&lt;/P&gt;&lt;P&gt;the size of ATA commands to avoid this scenario.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. The Lecroy analyzer can also emulate a device. Using this mode I&lt;/P&gt;&lt;P&gt;tried to trigger the issue with ATA commands. I couldn't figure out how&lt;/P&gt;&lt;P&gt;to trigger the exact scenario I wanted. I was able to cause the&lt;/P&gt;&lt;P&gt;response to be too short, just not short enough to underrun anything but&lt;/P&gt;&lt;P&gt;the last DMA buffer which doesn't seem to cause a problem. What I did&lt;/P&gt;&lt;P&gt;notice though was that this didn't seem to trigger an error anywhere in&lt;/P&gt;&lt;P&gt;the kernel or user space, the data would just simply be corrupted. I&lt;/P&gt;&lt;P&gt;would expect the system should flag the response as being invalid and an&lt;/P&gt;&lt;P&gt;IO error propagated all the way to user space.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 May 2015 19:47:58 GMT</pubDate>
    <dc:creator>Jon_Bagg</dc:creator>
    <dc:date>2015-05-19T19:47:58Z</dc:date>
    <item>
      <title>imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434237#M66343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Mounting a SATA CDROM fails aprox 1/20 times with this error....&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;root@freescale /tmp$ mount /dev/sr0 test/&lt;/P&gt;&lt;P&gt;UDF-fs: No partition found (1)&lt;/P&gt;&lt;P&gt;mount: mounting /dev/sr0 on test/ failed: Invalid argument&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using a Sabre imx6q board, freescale kernel 3.0.35 built with imx6_defconfig and the following extra configs&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CONFIG_BLK_DEV_SR=y&lt;/P&gt;&lt;P&gt;CONFIG_UDF_FS=y&lt;/P&gt;&lt;P&gt;CONFIG_UDF_NLS=y&lt;/P&gt;&lt;P&gt;CONFIG_ISO9660_FS=y&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried several disks and dvd drivers.&amp;nbsp; They all experience this issue on the Sabra board.&amp;nbsp; The same disks mount 100% of the time in an x86 machine.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I first noticed the issue on our own imx6d boards running mainline kernel 3.19.&amp;nbsp; Once in a while the kernel would dump out a backtrace (attached) when mounting.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335852"&gt;mount_cdrom_backtrace.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 16:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434237#M66343</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-04-22T16:15:55Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434238#M66344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I looked at your 3.19 logs and I would suggest you to report it to &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:linux-ide@vger.kernel.org"&gt;linux-ide@vger.kernel.org&lt;/A&gt;&lt;SPAN&gt; and &lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:linux-arm-kernel@lists.infradead.org"&gt;linux-arm-kernel@lists.infradead.org&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 16:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434238#M66344</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-04-22T16:23:50Z</dc:date>
    </item>
    <item>
      <title>Re: Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434239#M66345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; font-family: arial,helvetica,sans-serif;"&gt;Thanks Fabio.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: arial,helvetica,sans-serif; font-size: 10pt;"&gt;Customer &lt;SPAN style="color: #1f497d;"&gt;tried 3.19 on x86 to the same optical drive &amp;amp; disc and filesystem mounting is *&lt;STRONG&gt;not&lt;/STRONG&gt;* intermittent on that setup.&amp;nbsp; They will report this to the kernel folks.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-size: 10pt; font-family: arial,helvetica,sans-serif;"&gt;They are also going optical drive mounting with the same commands on i.MX53 and see what happens there.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 15:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434239#M66345</guid>
      <dc:creator>JohnBirch</dc:creator>
      <dc:date>2015-04-23T15:05:41Z</dc:date>
    </item>
    <item>
      <title>Re: Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434240#M66346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does it help to remove the UDF kernel options and mount it as&lt;/P&gt;&lt;P&gt;mount -t iso9660 /dev/sr0 /media/cdrom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 15:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434240#M66346</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-04-23T15:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434241#M66347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We've also discovered that cdparanoia will not function with audio disks on imx6 running mainline kernel, 3.19, 3.14 or 3.12.&amp;nbsp; This is 100% repeatable...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cdparanoia -vsQ&lt;/P&gt;&lt;P&gt;cdparanoia III release 10.2 (September 11, 2008)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using cdda library version: 10.2&lt;/P&gt;&lt;P&gt;Using paranoia library version: 10.2&lt;/P&gt;&lt;P&gt;Checking /dev/cdrom for cdrom...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Testing /dev/cdrom for SCSI/MMC interface&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SG_IO device: /dev/sr0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Drive is neither a CDROM nor a WORM device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Testing /dev/cdrom for cooked ioctl() interface&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /dev/sr0 is not a cooked ioctl CDROM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried the same CDROM drive, audio disk and root filesystem on a mx53 Quick Start Board using the same kernel and cdparanoia works fine.&amp;nbsp; The only differences were the mx53 device tree (imx53-qsb.dtb) and the load address (0x72000000) was changed before re-compiling the kernel (it just rebuilt uImage).&amp;nbsp; It appears the kernel's imx6 sata driver has some weird quirk with CDROMs or there is a bug in the imx6 sata silicon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cdparanoia -vsQ &lt;/P&gt;&lt;P&gt;cdparanoia III release 10.2 (September 11, 2008) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using cdda library version: 10.2 &lt;/P&gt;&lt;P&gt;Using paranoia library version: 10.2 &lt;/P&gt;&lt;P&gt;Checking /dev/cdrom for cdrom... &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Testing /dev/cdrom for SCSI/MMC interface &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SG_IO device: /dev/sr0 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CDROM model sensed sensed: TEAC DV-W28SS-B 1.2A &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking for SCSI emulation... &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Drive is ATAPI (using SG_IO host adaptor emulation) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checking for MMC style command set... &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Drive is MMC style &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DMA scatter/gather table entries: 1 &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; table entry size: 131072 bytes &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; maximum theoretical transfer: 55 sectors &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Setting default read size to 27 sectors (63504 bytes). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Verifying CDDA command set... &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Expected command set reads OK. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attempting to set cdrom to full speed... &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; drive returned OK. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Table of contents (audio tracks only): &lt;/P&gt;&lt;P&gt;track&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; length&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; begin&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; copy pre ch &lt;/P&gt;&lt;P&gt;=========================================================== &lt;/P&gt;&lt;P&gt;&amp;nbsp; 1.&amp;nbsp;&amp;nbsp;&amp;nbsp; 16305 [03:37.30]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 33 [00:00.33]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 2.&amp;nbsp;&amp;nbsp;&amp;nbsp; 49937 [11:05.62]&amp;nbsp;&amp;nbsp;&amp;nbsp; 16338 [03:37.63]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 3.&amp;nbsp;&amp;nbsp;&amp;nbsp; 29725 [06:36.25]&amp;nbsp;&amp;nbsp;&amp;nbsp; 66275 [14:43.50]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 4.&amp;nbsp;&amp;nbsp;&amp;nbsp; 14373 [03:11.48]&amp;nbsp;&amp;nbsp;&amp;nbsp; 96000 [21:20.00]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 5.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7302 [01:37.27]&amp;nbsp;&amp;nbsp; 110373 [24:31.48]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 6.&amp;nbsp;&amp;nbsp;&amp;nbsp; 12793 [02:50.43]&amp;nbsp;&amp;nbsp; 117675 [26:09.00]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 7.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 9785 [02:10.35]&amp;nbsp;&amp;nbsp; 130468 [28:59.43]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 8.&amp;nbsp;&amp;nbsp;&amp;nbsp; 19347 [04:17.72]&amp;nbsp;&amp;nbsp; 140253 [31:10.03]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;&amp;nbsp; 9.&amp;nbsp;&amp;nbsp;&amp;nbsp; 10928 [02:25.53]&amp;nbsp;&amp;nbsp; 159600 [35:28.00]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt; 10.&amp;nbsp;&amp;nbsp;&amp;nbsp; 33980 [07:33.05]&amp;nbsp;&amp;nbsp; 170528 [37:53.53]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt; 11.&amp;nbsp;&amp;nbsp;&amp;nbsp; 24910 [05:32.10]&amp;nbsp;&amp;nbsp; 204508 [45:26.58]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt; 12.&amp;nbsp;&amp;nbsp;&amp;nbsp; 19277 [04:17.02]&amp;nbsp;&amp;nbsp; 229418 [50:58.68]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt; 13.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7773 [01:43.48]&amp;nbsp;&amp;nbsp; 248695 [55:15.70]&amp;nbsp;&amp;nbsp;&amp;nbsp; no&amp;nbsp;&amp;nbsp; no&amp;nbsp; 2 &lt;/P&gt;&lt;P&gt;TOTAL&amp;nbsp; 256435 [56:59.10]&amp;nbsp;&amp;nbsp;&amp;nbsp; (audio only)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 15:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434241#M66347</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-08T15:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434242#M66348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Software setup for above comparison....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------[ Sabre Board setup ]------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;u-boot (2015.01-rc1-00014-g63f7af9)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;export PATH="$PATH:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/"&lt;/P&gt;&lt;P&gt;export ARCH=arm&lt;/P&gt;&lt;P&gt;export CROSS_COMPILE=arm-none-linux-gnueabi-&lt;/P&gt;&lt;P&gt;make mx6qsabresd_defconfig&lt;/P&gt;&lt;P&gt;make&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;kernel (3.19 or mainline)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;export PATH="$PATH:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/"&lt;/P&gt;&lt;P&gt;export ARCH=arm&lt;/P&gt;&lt;P&gt;export CROSS_COMPILE=arm-none-linux-gnueabi-&lt;/P&gt;&lt;P&gt;export LOADADDR=10008000&lt;/P&gt;&lt;P&gt;make imx_v6_v7_defconfig&lt;/P&gt;&lt;P&gt;make menuconfig&lt;/P&gt;&lt;P&gt;1. Enable CDROM support (Drivers -&amp;gt; SCSI device support -&amp;gt; SCSI CDROM support)&lt;/P&gt;&lt;P&gt;2. Enable CDROM file system support (File system -&amp;gt; CD-ROM/DVD Filesystems -&amp;gt; select all)&lt;/P&gt;&lt;P&gt;make uImage dtbs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sdcard (sdf in PC)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sudo dd if=arch/arm/boot/uImage of=/dev/sdf bs=512 seek=2048 &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;P&gt;sudo dd if=arch/arm/boot/dts/imx6q-sabresd.dtb of=/dev/sdf bs=512 seek=20480 &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;u-boot environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bootargs=console=ttymxc0,115200 root=/dev/mmcblk0p1&lt;/P&gt;&lt;P&gt;bootcmd=run bootargs; mmc dev 1; mmc read 0x12000000 0x800 0x2f00; mmc read 0x18000000 0x5000 0x100;bootm 0x12000000 - 0x18000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------[ imx53 Quick Start Board setup ]------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;u-boot (2015.01-rc1-00014-g63f7af9)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;export PATH="$PATH:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/"&lt;/P&gt;&lt;P&gt;export ARCH=arm&lt;/P&gt;&lt;P&gt;export CROSS_COMPILE=arm-none-linux-gnueabi-&lt;/P&gt;&lt;P&gt;make mx53loco_defconfig&lt;/P&gt;&lt;P&gt;make&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;kernel (3.19 or mainline)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;export PATH="$PATH:/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/"&lt;/P&gt;&lt;P&gt;export ARCH=arm&lt;/P&gt;&lt;P&gt;export CROSS_COMPILE=arm-none-linux-gnueabi-&lt;/P&gt;&lt;P&gt;export LOADADDR=72000000&lt;/P&gt;&lt;P&gt;make imx_v6_v7_defconfig&lt;/P&gt;&lt;P&gt;make menuconfig&lt;/P&gt;&lt;P&gt;1. Enable CDROM support (Drivers -&amp;gt; SCSI device support -&amp;gt; SCSI CDROM support)&lt;/P&gt;&lt;P&gt;2. Enable CDROM file system support (File system -&amp;gt; CD-ROM/DVD Filesystems -&amp;gt; select all)&lt;/P&gt;&lt;P&gt;make uImage dtbs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sdcard (sdf in PC)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sudo dd if=arch/arm/boot/uImage of=/dev/sdf bs=512 seek=2048 &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;P&gt;sudo dd if=arch/arm/boot/dts/imx53-qsb.dtb of=/dev/sdf bs=512 seek=20480 &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;u-boot environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bootargs=console=ttymxc0,115200 root=/dev/mmcblk0p1&lt;/P&gt;&lt;P&gt;bootcmd_mmc=run bootargs; mmc read 0x72000000 0x800 0x2f00; mmc read 0x71000000 0x5000 0x100; bootm 0x72000000 - 0x71000000&lt;/P&gt;&lt;P&gt;bootcmd=run bootcmd_mmc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 15:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434242#M66348</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-08T15:47:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434243#M66349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's interesting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you remove the SATA settings from include/configs/mx53loco.h?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define CONFIG_CMD_SATA&lt;/P&gt;&lt;P&gt;#ifdef CONFIG_CMD_SATA&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CONFIG_DWC_AHSATA&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CONFIG_SYS_SATA_MAX_DEVICE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CONFIG_DWC_AHSATA_PORT_ID&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CONFIG_DWC_AHSATA_BASE_ADDR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SATA_BASE_ADDR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CONFIG_LBA48&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define CONFIG_LIBATA&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to make sure that U-boot is not doing something to the SATA controller that 'fixes' the kernel issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 15:54:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434243#M66349</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-05-08T15:54:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434244#M66350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I commented out the whole CONFIG_CMD_SATA section, rebuilt and dd u-boot to the mx53 sdcard.&amp;nbsp; cdparanoia still works great.&amp;nbsp; Also, having a CDROM on a port multiplier on imx6 sabre breaks everything connected to the port multiplier.&amp;nbsp; The same port multiplier setup on the mx53-qsb works fine.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 16:39:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434244#M66350</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-08T16:39:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434245#M66351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am wondering if GP13 parameters need to be tweaked like done in arch/arm/boot/dts/imx6q-cubox-i.dts&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 16:46:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434245#M66351</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-05-08T16:46:10Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434246#M66352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had tried similar values...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &amp;amp;sata {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,transmit-level-mV = &amp;lt;1025&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,transmit-boost-mdB = &amp;lt;3330&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,transmit-atten-16ths = &amp;lt;9&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,receive-eq-mdB = &amp;lt;3000&amp;gt;;&lt;/P&gt;&lt;P&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me try the exact cubox's values on the Sabre.&amp;nbsp; We purchased a cubox to see if the CDROM worked, it has similar issues.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 17:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434246#M66352</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-08T17:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434247#M66353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I put&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;amp;sata {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; status = "okay";&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,transmit-level-mV = &amp;lt;1104&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,transmit-boost-mdB = &amp;lt;0&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,transmit-atten-16ths = &amp;lt;9&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,no-spread-spectrum;&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in arch/arm/boot/dts/imx6q-sabresd.dts.&amp;nbsp; cdparanoia is still very unhappy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 18:13:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434247#M66353</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-08T18:13:44Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434248#M66354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you apply ata_debug.patch, you can see some differences between the imx6 and imx53 when you run cdparanoia &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;dmesg | grep CDB&lt;/P&gt;&lt;P&gt;(note the time stamp on the last message to find the new one caused by cdparanoia )&lt;/P&gt;&lt;P&gt;cdparanoia -vsQ&lt;/P&gt;&lt;P&gt;dmesg | grep CDB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx53&lt;/P&gt;&lt;P&gt;ata_scsi_dump_cdb: CDB (1:0,0,-571258880) 00 00 4a 01 00 00 10 00 00&lt;/P&gt;&lt;P&gt;CDB rbuf: [4a 01 00 00 10 00 00 00 08]&lt;/P&gt;&lt;P&gt;CDB rbuf: 00000000: 00 06 04 56 00 02 00 00 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6 - third line is always zeros&lt;/P&gt;&lt;P&gt;ata_scsi_dump_cdb: CDB (1:0,0,-1122908160) 00 00 4a 01 00 00 10 00 00&lt;/P&gt;&lt;P&gt;CDB rbuf: [4a 01 00 00 10 00 00 00 08]&lt;/P&gt;&lt;P&gt;CDB rbuf: 00000000: 00 00 00 00 00 00 00 00&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 19:27:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434248#M66354</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-08T19:27:27Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434249#M66355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoPlainText" style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;I tried at my side on imx6q sd board, with the fsl's 3.14 kernel and v4.0-rc1 kernel, the cd-rom works.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoPlainText" style="margin: 0in 0in 0pt;"&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt; &lt;/SPAN&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;NOTE: The power supply of the DVD_ROM and so on, should be provide by the&lt;SPAN style="mso-spacerun: yes;"&gt;&amp;nbsp; &lt;/SPAN&gt;external PC power supply.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoPlainText" style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;I'm afraid that the power consumption of the DVD_ROM device is too huge to supplied by imx6q sd board itself.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoPlainText" style="margin: 0in 0in 0pt;"&gt; &lt;/P&gt;&lt;P class="MsoPlainText" style="margin: 0in 0in 0pt;"&gt;&lt;SPAN style="color: #000000; font-size: 12pt; font-family: Calibri;"&gt;Can you retry it when the external power supply is used?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: Times New Roman; font-size: 12pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;V4.0 -rc1&lt;/P&gt;&lt;P&gt;---------------logs----------------------&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# dmesg | grep ata&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Memory policy: Data cache writealloc&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Kernel command line: noinitrd console=ttymxc0,115200 mem=768M root=/dev/nfs nfsroot=10.192.224.44:/data/rootfs_home/r65037/yacto/rootfs_2014_310_110ga, tcp ip=dhcp no_console_suspend earlyprintk rw&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000] Memory: 743828K/786432K available (7211K kernel code, 388K rwdata, 2500K rodata, 372K init, 8350K bss, 26220K reserved, 16384K cma-reserved, 0K highmem)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.000000]&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x809e2000 - 0x80a432c0&amp;nbsp;&amp;nbsp; ( 389 kB)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.184484] libata version 3.00 loaded.&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.168019] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.175990] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.184034] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.192246] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.203138] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.210167] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.218980] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst &lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.235652] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 312&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.789195] ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 300)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.798035] ata1.00: ATAPI: HL-DT-ST DVD+/-RW GH50N, B103, max UDMA/100&lt;BR /&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.807626] ata1.00: configured for UDMA/100&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 10.676048] EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;[&amp;nbsp;&amp;nbsp; 10.700946] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.&lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# mount -t iso9660 /dev/sr0 /mnt/cdrom/&lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# df&lt;BR /&gt;Filesystem&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1K-blocks&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Used&amp;nbsp; Available Use% Mounted on&lt;BR /&gt;10.192.224.44:/data/rootfs_home/r65037/yacto/rootfs_2014_310_110ga 1922197336 673351608 1151180756&amp;nbsp; 37% /&lt;BR /&gt;devtmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 371912&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 371908&amp;nbsp;&amp;nbsp; 1% /dev&lt;BR /&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp; 0% /mnt/.psplash&lt;BR /&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380292&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380100&amp;nbsp;&amp;nbsp; 1% /run&lt;BR /&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380292&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 96&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380196&amp;nbsp;&amp;nbsp; 1% /var/volatile&lt;BR /&gt;/dev/mmcblk1p1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7494760&amp;nbsp;&amp;nbsp;&amp;nbsp; 432628&amp;nbsp;&amp;nbsp;&amp;nbsp; 6658372&amp;nbsp;&amp;nbsp; 7% /run/media/mmcblk1p1&lt;BR /&gt;/dev/mmcblk0p1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 117760&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 48&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 117712&amp;nbsp;&amp;nbsp; 1% /run/media/mmcblk0p1&lt;BR /&gt;/dev/sr0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7274&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7274&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 100% /mnt/cdrom&lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# uname -a&lt;BR /&gt;Linux imx6sxsabresd 4.0.0-rc1 #167 SMP Mon May 11 14:11:59 CST 2015 armv7l GNU/Linux&lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~#&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.14&lt;/P&gt;&lt;P&gt;----------------logs------------------------------&lt;/P&gt;&lt;P&gt; &lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# dmesg | grep ata&lt;BR /&gt;CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache&lt;BR /&gt;Memory policy: Data cache writealloc&lt;BR /&gt;Kernel command line: noinitrd console=ttymxc0,115200 mem=768M root=/dev/nfs nfsroot=10.192.224.44:/data/rootfs_home/r65037/yacto/rootfs_2014_310_110ga, tcp ip=dhcp no_console_suspend earlyprintk rw&lt;BR /&gt;Memory: 433184K/786432K available (7664K kernel code, 456K rwdata, 8744K rodata, 388K init, 438K bss, 353248K reserved, 0K highmem)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; .data : 0x81072000 - 0x810e42a0&amp;nbsp;&amp;nbsp; ( 457 kB)&lt;BR /&gt;libata version 3.00 loaded.&lt;BR /&gt;ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024&lt;BR /&gt;ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480&lt;BR /&gt;ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000&lt;BR /&gt;ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000&lt;BR /&gt;ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled&lt;BR /&gt;ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode&lt;BR /&gt;ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst &lt;BR /&gt;ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 71&lt;BR /&gt;ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 300)&lt;BR /&gt;ata1.00: ATAPI: HL-DT-ST DVD+/-RW GH50N, B103, max UDMA/100&lt;BR /&gt;ata1.00: configured for UDMA/100&lt;BR /&gt;mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed&lt;BR /&gt;FAT-fs (mmcblk2p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.&lt;BR /&gt;EXT4-fs (mmcblk3p1): mounted filesystem with ordered data mode. Opts: (null)&lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# mount -t iso9660 /dev/s&lt;BR /&gt;shm/&amp;nbsp;&amp;nbsp;&amp;nbsp; snd/&amp;nbsp;&amp;nbsp;&amp;nbsp; sr0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; stderr&amp;nbsp; stdin&amp;nbsp;&amp;nbsp; stdout&amp;nbsp; &lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# mount -t iso9660 /dev/sr0 /mnt/cdrom/&lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# df&lt;BR /&gt;Filesystem&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1K-blocks&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Used&amp;nbsp; Available Use% Mounted on&lt;BR /&gt;10.192.224.44:/data/rootfs_home/r65037/yacto/rootfs_2014_310_110ga 1922197336 673337648 1151194716&amp;nbsp; 37% /&lt;BR /&gt;devtmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 216592&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 216588&amp;nbsp;&amp;nbsp; 1% /dev&lt;BR /&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp; 0% /mnt/.psplash&lt;BR /&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380624&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 276&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380348&amp;nbsp;&amp;nbsp; 1% /run&lt;BR /&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380624&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 96&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380528&amp;nbsp;&amp;nbsp; 1% /var/volatile&lt;BR /&gt;/dev/mmcblk2p1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 117760&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 48&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 117712&amp;nbsp;&amp;nbsp; 1% /run/media/mmcblk2p1&lt;BR /&gt;/dev/mmcblk3p1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7494760&amp;nbsp;&amp;nbsp;&amp;nbsp; 432628&amp;nbsp;&amp;nbsp;&amp;nbsp; 6658372&amp;nbsp;&amp;nbsp; 7% /run/media/mmcblk3p1&lt;BR /&gt;/dev/sr0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7274&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7274&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 100% /mnt/cdrom&lt;BR /&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# ls /mnt/cdrom/ -lt&lt;BR /&gt;total 4518&lt;BR /&gt;-r-xr-xr-x 1 root root 4423701 Jan 21&amp;nbsp; 2010 WT_3978.exe&lt;BR /&gt;-r-xr-xr-x 1 root root&amp;nbsp; 190989 Jan 21&amp;nbsp; 2010 WT_3978.swf&lt;BR /&gt;dr-xr-xr-x 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp; 2048 Jan 18&amp;nbsp; 2010 fscommand&lt;BR /&gt;dr-xr-xr-x 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp; 2048 Dec 22&amp;nbsp; 2009 files&lt;BR /&gt;dr-xr-xr-x 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp; 2048 Dec 22&amp;nbsp; 2009 Scripts&lt;BR /&gt;-r-xr-xr-x 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp; 1653 Dec 22&amp;nbsp; 2009 WT_3978.html&lt;BR /&gt;-r-xr-xr-x 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 49 Dec 22&amp;nbsp; 2009 AUTORUN.INF&lt;BR /&gt;-r-xr-xr-x 1 root root&amp;nbsp;&amp;nbsp;&amp;nbsp; 1150 May 20&amp;nbsp; 2008 freescale.ico&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Linux version 3.14.38-02099-g22acdbb (&lt;A href="mailto:r65037@shlinux2"&gt;r65037@shlinux2&lt;/A&gt;) (gcc version 4.8.2 (GCC) ) #330 SMP PREEMPT Mon May 11 13:40:26 CST 2015&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2015 08:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434249#M66355</guid>
      <dc:creator>richard_zhu</dc:creator>
      <dc:date>2015-05-11T08:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434250#M66356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;Hongxing,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;I can also get the CDROM to mount on the imx6q-sabre, just not 100% of the time.&amp;nbsp; Please try&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;cdparanoia -vsQ&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;with an audio CD and see if you can get a track listing on your setup as it is 100 failure / reproducible on our setup.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2015 13:13:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434250#M66356</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-11T13:13:38Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434251#M66357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just a suggestion:&lt;/P&gt;&lt;P&gt;Could you share your rootfs with cdparanoia application installed? That would makes things easier for Richard to reproduce.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2015 13:25:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434251#M66357</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2015-05-11T13:25:07Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434252#M66358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="https://lenbrook.sharefile.com/d-s59f1181de4f466eb" title="https://lenbrook.sharefile.com/d-s59f1181de4f466eb"&gt;https://lenbrook.sharefile.com/d-s59f1181de4f466eb&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. You'll have to replace the password file before booting&lt;/P&gt;&lt;P&gt;2. comment out this line&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/etc/rc.d/rc.sovi &amp;amp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;at the end of /etc/rc.d/rcS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if [[ -e /var/data/intertek ]]; then&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mount -o remount junk /&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /usr/bin/etf_serv &amp;amp;&lt;/P&gt;&lt;P&gt;else&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; # start sovi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; # /etc/rc.d/rc.sovi &amp;amp;&lt;/P&gt;&lt;P&gt;fi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2015 13:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434252#M66358</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-11T13:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434253#M66359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan:&lt;/P&gt;&lt;P&gt;Sorry, I can't download the rootfs pasted above.&lt;BR /&gt;It reports the following info. :smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="title"&gt;This page can't be displayed&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Make sure the web address &lt;SPAN class="webpageURL"&gt;&lt;A class="jive-link-external-small" href="https://lenbrook.sharefile.com" rel="nofollow" target="_blank"&gt;https://lenbrook.sharefile.com&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;is correct.&lt;/LI&gt;&lt;LI&gt;Look for the page with your search engine.&lt;/LI&gt;&lt;LI&gt;Refresh the page in a few minutes.&lt;/LI&gt;&lt;LI&gt;Make sure TLS and SSL protocols are enabled. Go to Tools &amp;gt; Internet Options &amp;gt; Advanced &amp;gt; Settings &amp;gt; Security&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway,&amp;nbsp; did you ever do the tests with the external power supply?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I did is listed below, the mount operations can be finished successfuly, although there maybe mount failure on the first mount sometimes.&lt;/P&gt;&lt;P&gt;both board and dvd_rom is powered off --&amp;gt; boot up board--&amp;gt; power on dvd_rom --&amp;gt; kernel booting--&amp;gt; mount dvd_rom.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The logs when there maybe mount failure on the first mount sometimes.&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# mount /dev/sr0 /mnt/cdrom/&lt;/P&gt;&lt;P&gt;UDF-fs: warning (device sr0): udf_fill_super: No partition found (2)&lt;/P&gt;&lt;P&gt;mount: mounting /dev/sr0 on /mnt/cdrom/ failed: Invalid argument&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# mount /dev/sr0 /mnt/cdrom/&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~# df&lt;/P&gt;&lt;P&gt;Filesystem&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1K-blocks&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Used&amp;nbsp; Available Use% Mounted on&lt;/P&gt;&lt;P&gt;10.192.224.44:/data/rootfs_home/r65037/yacto/rootfs_2014_310_110ga 1922197336 673339540 1151192824&amp;nbsp; 37% /&lt;/P&gt;&lt;P&gt;devtmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 216592&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 216588&amp;nbsp;&amp;nbsp; 1% /dev&lt;/P&gt;&lt;P&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 40&amp;nbsp;&amp;nbsp; 0% /mnt/.psplash&lt;/P&gt;&lt;P&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380624&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 276&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380348&amp;nbsp;&amp;nbsp; 1% /run&lt;/P&gt;&lt;P&gt;tmpfs&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380624&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 96&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 380528&amp;nbsp;&amp;nbsp; 1% /var/volatile&lt;/P&gt;&lt;P&gt;/dev/mmcblk3p1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7494760&amp;nbsp;&amp;nbsp;&amp;nbsp; 432628&amp;nbsp;&amp;nbsp;&amp;nbsp; 6658372&amp;nbsp;&amp;nbsp; 7% /run/media/mmcblk3p1&lt;/P&gt;&lt;P&gt;/dev/mmcblk2p1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 117760&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 48&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 117712&amp;nbsp;&amp;nbsp; 1% /run/media/mmcblk2p1&lt;/P&gt;&lt;P&gt;/dev/sr0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7274&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7274&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 100% /mnt/cdrom&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@imx6sxsabresd"&gt;root@imx6sxsabresd&lt;/A&gt;:~#&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 02:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434253#M66359</guid>
      <dc:creator>richard_zhu</dc:creator>
      <dc:date>2015-05-12T02:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434254#M66360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both my boss and I tested the link and it is ok.&amp;nbsp; If you are still unsuccessful, please let me know and I try something else.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Over the past several weeks I have had multiple ways of powering the CDROM....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. slim drive CDROM connected to sabre&lt;/P&gt;&lt;P&gt;2. slim drive CDROM powered from external supply&lt;/P&gt;&lt;P&gt;3. full 5-1/4" CDROM +12v powered from external supply&lt;/P&gt;&lt;P&gt;4. full 5-1/4" CDROM +5v &amp;amp; +12v powered from external supply when using port multiplier.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 12:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434254#M66360</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-12T12:38:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434255#M66361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My co-worker discovered something interesting....Using a kernel with ata_debug.patch applied he noticed that before there is any file system access or cdparanoia usage, on the imx6 the cdrom's response to command "4a" (GET_EVENT_STATUS_NOTIFICATION) is always corrupted / random on the imx6 and not the imx53.&amp;nbsp; The first two bytes of the response are the length and should always be 00 06. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx53&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.713046] CDB rbuf: [4a 01 00 00 10 00 00 00 08]&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.717849] CDB rbuf: 00000000: 00 06 04 56 00 02 00 00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;imx6&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.451017] CDB rbuf: [4a 01 00 00 10 00 00 00 08]&lt;/P&gt;&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.451024] CDB rbuf: 00000000: 01 a0 20 48 6f d6 f6 b5&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;He also discovered that changing the length of the previous command [&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 3.422134] CDB rbuf: [5a 00 2a 00 00 00 00 00 80] from 80 to 40, the "4a" will then succeed on the imx6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 13:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434255#M66361</guid>
      <dc:creator>Jon_Bagg</dc:creator>
      <dc:date>2015-05-12T13:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: imx6 sata cdrom driver issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434256#M66362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joanthan:&lt;BR /&gt;Thanks for your debug efforts firstly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I received your rootfs today, but I failed to login although I replace the passwd and masked the rc.sovi line in rcS.&lt;/P&gt;&lt;P&gt;Do you know the passwd of user(18DF)?&lt;/P&gt;&lt;P&gt;Here is the log:&lt;/P&gt;&lt;P&gt;Known &amp;lt;ldisc&amp;gt; names:&lt;BR /&gt;&amp;nbsp; TTY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SLIP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MOUSE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PPP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; STRIP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; AX25&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; X25&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 6PACK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; R3964&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IRDA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HDLC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SYNC_PPP&amp;nbsp; &lt;BR /&gt;&amp;nbsp; SYNCPPP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HCI&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PPS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; M101&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GIGASET&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GIGASET_M101&lt;/P&gt;&lt;P&gt;Known &amp;lt;iflag&amp;gt; names:&lt;BR /&gt;&amp;nbsp; IGNBRK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BRKINT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IGNPAR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PARMRK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; INPCK&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ISTRIP&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; INLCR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IGNCR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ICRNL&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IUCLC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IXON&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IXANY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp; IXOFF&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IMAXBEL&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; IUTF8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;For more details see ldattach(8).&lt;BR /&gt;I/O warning : failed to load external entity "/etc/sovi_info.xml"&lt;BR /&gt;Failed to create client object: Daemon not running&lt;BR /&gt;I/O warning : failed to load external entity "/etc/sovi_info.xml"&lt;BR /&gt;sed: /etc/sovi_info.xml: No such file or directory&lt;BR /&gt;sed: /var/avahi/services/*: No such file or directory&lt;BR /&gt;Error connecting: Error connecting: No such file or directory&lt;BR /&gt;I/O warning : failed to load external entity "/etc/sovi_info.xml"&lt;BR /&gt;/etc/rc.d/rcS: line 84:&amp;nbsp; 1310 Segmentation fault&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; sovi_hal&lt;BR /&gt;modprobe: chdir(3.14.38-02099-g22acdbb): No such file or directory&lt;BR /&gt;File does not exist: /etc/sovi_info.xml at /etc/rc.d/rc.alsa line 7&lt;BR /&gt;Generating keys for the dropbear ssh server: &lt;BR /&gt;Will output 1024 bit rsa secret key to '/var/data/etc/dropbear_rsa_host_key'&lt;BR /&gt;Generating key, this may take a while...&lt;BR /&gt;Public key portion is:&lt;BR /&gt;ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAAAgwDjcQUsMQMlmQhVD9bYmLQno77/iJXp9N1Zz3fEkgC588Jy/4+mML7xubqN+zucmtLDh9ND0LPFc0vy4+AwZ4QRB6kmeeZuGhqevUE+poElsvzOZz7daAwMfy8hY6DZ2O7JP7V9sj5lfj/ar993bkyEvob8Bj4V7NZlZ47V0+ee81nL &lt;A href="mailto:root@18DF"&gt;root@18DF&lt;/A&gt;&lt;BR /&gt;Fingerprint: md5 93:f8:d5:5a:9a:7c:e0:30:1d:37:24:01:8c:2e:97:2c&lt;BR /&gt;Start dropbear ssh server&lt;BR /&gt;sed: /etc/sovi_info.xml: No such file or directory&lt;BR /&gt;Unknown group "netdev" in message bus configuration file&lt;BR /&gt;~~~~mask rc.sovi~~~~&lt;BR /&gt;All done&lt;BR /&gt;starting pid 1341, tty '': '/sbin/getty -L ttymxc0 115200 vt100'&lt;BR /&gt;sed: /etc/sovi_info.xml: No such file or directory&lt;BR /&gt;sed: /etc/sovi_info.xml: No such file or directory&lt;BR /&gt;avahi-browser-sovi 0.5&lt;/P&gt;&lt;P&gt;18DF login: Could not open sovi_info.xml &lt;/P&gt;&lt;P&gt;18DF login: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, it seems that the dvd_rom works refer to the boot log of kernel:&lt;/P&gt;&lt;P&gt;......&lt;/P&gt;&lt;P&gt;ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 300)&lt;/P&gt;&lt;P&gt;ata1.00: ATAPI: HL-DT-ST DVD+/-RW GH50N, B103, max UDMA/100&lt;/P&gt;&lt;P&gt;ata1.00: configured for UDMA/100&lt;/P&gt;&lt;P&gt;mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA&lt;/P&gt;&lt;P&gt;mmc2: no vqmmc regulator found&lt;/P&gt;&lt;P&gt;mmc2: no vmmc regulator found&lt;/P&gt;&lt;P&gt;scsi 0:0:0:0: CD-ROM&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; HL-DT-ST DVD+-RW GH50N&amp;nbsp;&amp;nbsp;&amp;nbsp; B103 PQ: 0 ANSI: 5&lt;/P&gt;&lt;P&gt;sr0: scsi3-mmc drive: 48x/48x writer dvd-ram cd/rw xa/form2 cdda tray&lt;/P&gt;&lt;P&gt;cdrom: Uniform CD-ROM driver Revision: 3.20&lt;/P&gt;&lt;P&gt;......&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 03:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6-sata-cdrom-driver-issue/m-p/434256#M66362</guid>
      <dc:creator>richard_zhu</dc:creator>
      <dc:date>2015-05-13T03:01:42Z</dc:date>
    </item>
  </channel>
</rss>