<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 How can I program MMPF0100NP to F0 mode in u-boot?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-program-MMPF0100NP-to-F0-mode-in-u-boot/m-p/433990#M66313</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In u-boot console, I excuted 'i2c probe' and confirmed communication with PMIC(0x08 i2c line).&lt;/P&gt;&lt;P&gt;But there are so many parameters that I have a hard time to test.&lt;/P&gt;&lt;P&gt;If there are references for setting PMIC to F0 mode, please tell me how can I get them.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jun 2015 09:01:25 GMT</pubDate>
    <dc:creator>JHY</dc:creator>
    <dc:date>2015-06-26T09:01:25Z</dc:date>
    <item>
      <title>How can I program MMPF0100NP to F0 mode in u-boot?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-program-MMPF0100NP-to-F0-mode-in-u-boot/m-p/433990#M66313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In u-boot console, I excuted 'i2c probe' and confirmed communication with PMIC(0x08 i2c line).&lt;/P&gt;&lt;P&gt;But there are so many parameters that I have a hard time to test.&lt;/P&gt;&lt;P&gt;If there are references for setting PMIC to F0 mode, please tell me how can I get them.&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2015 09:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-program-MMPF0100NP-to-F0-mode-in-u-boot/m-p/433990#M66313</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-06-26T09:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: How can I program MMPF0100NP to F0 mode in u-boot?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-I-program-MMPF0100NP-to-F0-mode-in-u-boot/m-p/433991#M66314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please refer to&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/analog/doc/app_note/AN4536.pdf?fasp=1&amp;amp;WT_TYPE=Application%20Notes&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;AN4536&lt;/A&gt; AN4536, MMPF0100 OTP Programming Instructions - Application Note&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2015 10:55:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-I-program-MMPF0100NP-to-F0-mode-in-u-boot/m-p/433991#M66314</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-26T10:55:45Z</dc:date>
    </item>
  </channel>
</rss>