<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx.6 SABRESD with mag3110 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-SABRESD-with-mag3110/m-p/433772#M66246</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the fsl-image-gui image generate in Yocto.&lt;/P&gt;&lt;P&gt;This one contains the evtest-capture program that you can use to test the magnetometer.&lt;/P&gt;&lt;P&gt;Also you can check the configuration in the imx6qdl-sabresd.dtsi file, like the i2c port used and the gpio pin used for the irq.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Apr 2015 21:43:57 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2015-04-27T21:43:57Z</dc:date>
    <item>
      <title>imx.6 SABRESD with mag3110</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-SABRESD-with-mag3110/m-p/433771#M66245</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using SABRESD board, is anyone successful in using mag3110 magnetometer. Does it required to do any rework on the board.&lt;/P&gt;&lt;P&gt;Does anyone share the I2C Master configuration values to get acknowledgement from mag3110. Can anyone share the pad and mux &lt;/P&gt;&lt;P&gt;configuration for mag3110 on I2C3. Please do needful&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 15:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-SABRESD-with-mag3110/m-p/433771#M66245</guid>
      <dc:creator>bottleneck</dc:creator>
      <dc:date>2015-04-22T15:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: imx.6 SABRESD with mag3110</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-6-SABRESD-with-mag3110/m-p/433772#M66246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the fsl-image-gui image generate in Yocto.&lt;/P&gt;&lt;P&gt;This one contains the evtest-capture program that you can use to test the magnetometer.&lt;/P&gt;&lt;P&gt;Also you can check the configuration in the imx6qdl-sabresd.dtsi file, like the i2c port used and the gpio pin used for the irq.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2015 21:43:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-6-SABRESD-with-mag3110/m-p/433772#M66246</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-04-27T21:43:57Z</dc:date>
    </item>
  </channel>
</rss>