<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Freescale kernel roadmap ? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433555#M66192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Stuart Adams,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One of the git trees is part of the FSL Community BSP (git://github.com/Freescale/linux-fslc), which is always changing and open for contributions so it is more up-to-date in a sense. This tree is part of the Yocto Project. You may find relatively new kernel versions available even for processors released a while ago. Some third party boards are also covered on this BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other tree (git://git.freescale.com/imx/linux-2.6-imx.git) is part of the BSP Release, which is static and only support the machines listed on the Release Notes. These are the official releases and do not change as much as the FSL Community BSP. Usually older processors do not have new BSPs releases planned so not all processors will be migrated to newer kernel versions. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information about the roadmap of the BSP Releases for a family of processors please contact your local FSL Representative who will gladly help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Nov 2015 19:27:47 GMT</pubDate>
    <dc:creator>gusarambula</dc:creator>
    <dc:date>2015-11-26T19:27:47Z</dc:date>
    <item>
      <title>Freescale kernel roadmap ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433554#M66191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the freescale roadmap for the kernel ??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As of the latest yocto recipes there are currently two git trees git://github.com/Freescale/linux-fslc.git and git://git.freescale.com/imx/linux-2.6-imx.git&lt;/P&gt;&lt;P&gt;default builds have mxs and mx5 platforms point to linux-fslc kernel version 4.1, mx6 to linux-fslc kernel 3.14-1 and mx6ul to linux-imx 3.14.38&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just wondering what the future direction is going to be ??&lt;/P&gt;&lt;P&gt;Will all imx platforms be moving to linux-fslc tree and kernel version 4.3x ??&lt;/P&gt;&lt;P&gt;(And what is the time frame consolidation ?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Stuart&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Nov 2015 15:50:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433554#M66191</guid>
      <dc:creator>SJA</dc:creator>
      <dc:date>2015-11-23T15:50:43Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale kernel roadmap ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433555#M66192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Stuart Adams,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One of the git trees is part of the FSL Community BSP (git://github.com/Freescale/linux-fslc), which is always changing and open for contributions so it is more up-to-date in a sense. This tree is part of the Yocto Project. You may find relatively new kernel versions available even for processors released a while ago. Some third party boards are also covered on this BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other tree (git://git.freescale.com/imx/linux-2.6-imx.git) is part of the BSP Release, which is static and only support the machines listed on the Release Notes. These are the official releases and do not change as much as the FSL Community BSP. Usually older processors do not have new BSPs releases planned so not all processors will be migrated to newer kernel versions. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information about the roadmap of the BSP Releases for a family of processors please contact your local FSL Representative who will gladly help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Nov 2015 19:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433555#M66192</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-11-26T19:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale kernel roadmap ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433556#M66193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I wondering what would be the best practice to start a new project ? In case of imx6UL should I take the &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;FSL Community kernel source or the one from freescale &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;BSP Release (which is defined as default for this evk board) ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 11:11:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433556#M66193</guid>
      <dc:creator>matt67</dc:creator>
      <dc:date>2016-03-30T11:11:20Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale kernel roadmap ?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433557#M66194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello matt67,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you may find the following conversation useful. There is no right answer and it will most likely depend on your project needs, but there are some guidelines to consider as mentioned there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/385542"&gt;i.MX6: Using kernel from Linus mainline instead of Freescale git&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Mar 2016 14:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Freescale-kernel-roadmap/m-p/433557#M66194</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2016-03-30T14:46:25Z</dc:date>
    </item>
  </channel>
</rss>