<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX6 CPUFREQ driver vs thermal driver. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CPUFREQ-driver-vs-thermal-driver/m-p/432114#M65798</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6 CPU frequency scaling and thermal control.&lt;/P&gt;&lt;P&gt;I know the CPU frequency is held to max frequency by the following command with L3.10.17_1.0.0-ga by CPUFREQ driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; echo performance &amp;gt; /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I know the CPU frequency is set to lower when the CPU temperature is over "passive point" for cooling by thermal driver also.&lt;/P&gt;&lt;P&gt;Then, which has a priority?&lt;/P&gt;&lt;P&gt;If scaling_governor is set to performance with the above command and CPU temperature is over "passive point", CPU frequency is kept to max frequency by CPUFREQ driver? or set to lower frequency by thermal driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Sep 2015 02:50:09 GMT</pubDate>
    <dc:creator>satoshishimoda</dc:creator>
    <dc:date>2015-09-08T02:50:09Z</dc:date>
    <item>
      <title>i.MX6 CPUFREQ driver vs thermal driver.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CPUFREQ-driver-vs-thermal-driver/m-p/432114#M65798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about i.MX6 CPU frequency scaling and thermal control.&lt;/P&gt;&lt;P&gt;I know the CPU frequency is held to max frequency by the following command with L3.10.17_1.0.0-ga by CPUFREQ driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; echo performance &amp;gt; /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I know the CPU frequency is set to lower when the CPU temperature is over "passive point" for cooling by thermal driver also.&lt;/P&gt;&lt;P&gt;Then, which has a priority?&lt;/P&gt;&lt;P&gt;If scaling_governor is set to performance with the above command and CPU temperature is over "passive point", CPU frequency is kept to max frequency by CPUFREQ driver? or set to lower frequency by thermal driver?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Satoshi Shimoda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 02:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CPUFREQ-driver-vs-thermal-driver/m-p/432114#M65798</guid>
      <dc:creator>satoshishimoda</dc:creator>
      <dc:date>2015-09-08T02:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6 CPUFREQ driver vs thermal driver.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CPUFREQ-driver-vs-thermal-driver/m-p/432115#M65799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Satoshi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Performance" governor will keep the CPU at the highest possible frequency,&lt;/P&gt;&lt;P&gt;ignoring temperature "points". Short description can be found on&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://idebian.wordpress.com/2008/06/22/cpu-frequency-scaling-in-linux/" title="https://idebian.wordpress.com/2008/06/22/cpu-frequency-scaling-in-linux/"&gt;CPU frequency scaling in Linux | iDebian's Weblog&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 04:20:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX6-CPUFREQ-driver-vs-thermal-driver/m-p/432115#M65799</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-08T04:20:01Z</dc:date>
    </item>
  </channel>
</rss>