<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UBIFS error on freescale linux kernel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431921#M65767</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Smitha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, nand can be corrupted after&lt;/P&gt;&lt;P&gt;sudden power loss, for example when power adapter is turned off.&lt;/P&gt;&lt;P&gt;Recommended to execute linux poweroff command&lt;/P&gt;&lt;P&gt;for finishing job. I am afraid it is not possible to retrieve data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 06 Jun 2015 00:44:19 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-06T00:44:19Z</dc:date>
    <item>
      <title>UBIFS error on freescale linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431920#M65766</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a freescale linux(2.6) kernel. We are using the mtd devices to communicate with the Micron Nand Flash memory. We suddenly started to see some problems with the UBIFS.&lt;/P&gt;&lt;P&gt;We are mounting the rootfs on mtd4 and the logfs on mtd5.&lt;/P&gt;&lt;P&gt;The error we see in the logs is:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Jan&amp;nbsp; 1 00:00:05 STX-16 user.notice kernel: klogd started: BusyBox v1.20.0 (2012-09-18 17:42:52 MST)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;.....&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;user.err kernel: UBIFS error (pid 1119): ubifs_recover_leb: LEB 24 scanning failed&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The partition seems to be corrupt. When does this happen? I have read that it happens during a power loss in some scenarios.&lt;/P&gt;&lt;P&gt;Also, is there a way to retrieve data? The roots seems ok because the logging information is being handled by the logfs partition. I am unable to mount the logfs partition. &lt;/P&gt;&lt;P&gt;When I try to mount mtd5, I get an error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mount: mounting ubi1:log on /mnt/nand failed: Structure needs cleaning&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Smitha.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2015 03:46:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431920#M65766</guid>
      <dc:creator>smitharatnam</dc:creator>
      <dc:date>2015-06-05T03:46:58Z</dc:date>
    </item>
    <item>
      <title>Re: UBIFS error on freescale linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431921#M65767</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Smitha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you are right, nand can be corrupted after&lt;/P&gt;&lt;P&gt;sudden power loss, for example when power adapter is turned off.&lt;/P&gt;&lt;P&gt;Recommended to execute linux poweroff command&lt;/P&gt;&lt;P&gt;for finishing job. I am afraid it is not possible to retrieve data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jun 2015 00:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431921#M65767</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-06T00:44:19Z</dc:date>
    </item>
    <item>
      <title>Re: UBIFS error on freescale linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431922#M65768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We dont know when there would be sudden power loss.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When do we use the power off command?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Jun 2015 05:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431922#M65768</guid>
      <dc:creator>smitharatnam</dc:creator>
      <dc:date>2015-06-06T05:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: UBIFS error on freescale linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431923#M65769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;power off command is used for finishing job.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 15:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431923#M65769</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-08T15:16:54Z</dc:date>
    </item>
    <item>
      <title>Re: UBIFS error on freescale linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431924#M65770</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you paste the command here? I am starting into all this recently.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can the power off command be part of the linux kernel files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Smitha.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 20:23:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431924#M65770</guid>
      <dc:creator>smitharatnam</dc:creator>
      <dc:date>2015-06-08T20:23:41Z</dc:date>
    </item>
    <item>
      <title>Re: UBIFS error on freescale linux kernel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431925#M65771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A href="http://linux.about.com/library/cmd/blcmdl8_poweroff.htm" title="http://linux.about.com/library/cmd/blcmdl8_poweroff.htm"&gt;poweroff - Linux Command - Unix Command&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 00:56:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/UBIFS-error-on-freescale-linux-kernel/m-p/431925#M65771</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-09T00:56:56Z</dc:date>
    </item>
  </channel>
</rss>