<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: PMIC POR_B  Delay</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-POR-B-Delay/m-p/431912#M65765</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Katrina&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use solution used in i.MX6SL EVK, spf-27452&amp;nbsp;&amp;nbsp; p.13&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6SLEVK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;iMX6SL_EVK_DESIGNFILES&lt;/A&gt;&amp;nbsp; : Design files, including hardware schematics&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58256iC20AC591727AB767/image-size/large?v=v2&amp;amp;px=999" title="spf-27452   p.13.jpg" alt="spf-27452   p.13.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jun 2015 00:28:05 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-26T00:28:05Z</dc:date>
    <item>
      <title>PMIC POR_B  Delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-POR-B-Delay/m-p/431911#M65764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;How long after the PMIC POR_B is released from low to high does it take to read the config bits? Since we use a mux (FET switch) on these lines which are also used as the EIM interface to the FPGA we need to ensure we hold the enable signal to this low long enough.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; font-family: 'Arial','sans-serif';"&gt;I tried tying POR_B directly to the mux so it releases on the same edge as the i.MX6. (It says somewhere that these are sampled on the edge of por_B rising. It won’t boot in this case. This mux enable needs to be delayed for some amount of time and I need to know how long that is..&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 18:29:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-POR-B-Delay/m-p/431911#M65764</guid>
      <dc:creator>katrinagundal-z</dc:creator>
      <dc:date>2015-06-25T18:29:20Z</dc:date>
    </item>
    <item>
      <title>Re: PMIC POR_B  Delay</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PMIC-POR-B-Delay/m-p/431912#M65765</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Katrina&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can use solution used in i.MX6SL EVK, spf-27452&amp;nbsp;&amp;nbsp; p.13&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6SLEVK&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;iMX6SL_EVK_DESIGNFILES&lt;/A&gt;&amp;nbsp; : Design files, including hardware schematics&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58256iC20AC591727AB767/image-size/large?v=v2&amp;amp;px=999" title="spf-27452   p.13.jpg" alt="spf-27452   p.13.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2015 00:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PMIC-POR-B-Delay/m-p/431912#M65765</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-26T00:28:05Z</dc:date>
    </item>
  </channel>
</rss>