<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX6 Sabre Lite Ubuntu Booting in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Sabre-Lite-Ubuntu-Booting/m-p/431885#M65759</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Kishore&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest to use ip=none as kernel boot parameter&lt;/P&gt;&lt;P&gt;and set ethaddr in uboot&lt;/P&gt;&lt;P&gt;&lt;A href="http://lists.denx.de/pipermail/u-boot/2007-July/023386.html" title="http://lists.denx.de/pipermail/u-boot/2007-July/023386.html"&gt;[U-Boot-Users] Changing ethaddr&lt;/A&gt; &lt;/P&gt;&lt;P&gt;ubuntu for this board is described on&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/" title="http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/"&gt;http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jun 2015 00:37:39 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-06-26T00:37:39Z</dc:date>
    <item>
      <title>IMX6 Sabre Lite Ubuntu Booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Sabre-Lite-Ubuntu-Booting/m-p/431884#M65758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just followed the procedure given in Sabre Lite wiki page to boot linux ( Ubuntu 14.0.4 ) for Sabre Lite Board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, When I power up the device SD card inserted. I am getting the below error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please tell me where I am doing wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2014.04-00123-g63ae4a5 (May 14 2014 - 17:09:55)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; Freescale i.MX6Q rev1.2 at 792 MHz&lt;/P&gt;&lt;P&gt;Reset cause: POR&lt;/P&gt;&lt;P&gt;Board: SABRE Lite&lt;/P&gt;&lt;P&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 1 GiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0, FSL_SDHC: 1&lt;/P&gt;&lt;P&gt;*** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No panel detected: default to HDMI&lt;/P&gt;&lt;P&gt;Display: HDMI (1024x768)&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; using phy at 6&lt;/P&gt;&lt;P&gt;FEC [PRIME]&lt;/P&gt;&lt;P&gt;Warning: failed to set MAC address&lt;/P&gt;&lt;P&gt;, usb_ether&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0 &lt;/P&gt;&lt;P&gt;mmc0 is current device&lt;/P&gt;&lt;P&gt;** Unrecognized filesystem type **&lt;/P&gt;&lt;P&gt;** Unrecognized filesystem type **&lt;/P&gt;&lt;P&gt;Booting from net ...&lt;/P&gt;&lt;P&gt;FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;/P&gt;&lt;P&gt;*** ERROR: `ethaddr' not set&lt;/P&gt;&lt;P&gt;ERROR: Need valid 'usbnet_devaddr' to be set&lt;/P&gt;&lt;P&gt;at drivers/usb/gadget/ether.c:2362/usb_eth_init()&lt;/P&gt;&lt;P&gt;FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;/P&gt;&lt;P&gt;FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;/P&gt;&lt;P&gt;*** ERROR: `ethaddr' not set&lt;/P&gt;&lt;P&gt;ERROR: Need valid 'usbnet_devaddr' to be set&lt;/P&gt;&lt;P&gt;at drivers/usb/gadget/ether.c:2362/usb_eth_init()&lt;/P&gt;&lt;P&gt;FEC Waiting for PHY auto negotiation to complete......... TIMEOUT !&lt;/P&gt;&lt;P&gt;Wrong Image Format for bootm command&lt;/P&gt;&lt;P&gt;ERROR: can't get kernel image!&lt;/P&gt;&lt;P&gt;U-Boot &amp;gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 15:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Sabre-Lite-Ubuntu-Booting/m-p/431884#M65758</guid>
      <dc:creator>venkatakishore</dc:creator>
      <dc:date>2015-06-25T15:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 Sabre Lite Ubuntu Booting</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-Sabre-Lite-Ubuntu-Booting/m-p/431885#M65759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Kishore&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would suggest to use ip=none as kernel boot parameter&lt;/P&gt;&lt;P&gt;and set ethaddr in uboot&lt;/P&gt;&lt;P&gt;&lt;A href="http://lists.denx.de/pipermail/u-boot/2007-July/023386.html" title="http://lists.denx.de/pipermail/u-boot/2007-July/023386.html"&gt;[U-Boot-Users] Changing ethaddr&lt;/A&gt; &lt;/P&gt;&lt;P&gt;ubuntu for this board is described on&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/" title="http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/"&gt;http://boundarydevices.com/running-linaro-ubuntu-on-i-mx6-sabre-lite-and-nitrogen6x/&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jun 2015 00:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-Sabre-Lite-Ubuntu-Booting/m-p/431885#M65759</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-26T00:37:39Z</dc:date>
    </item>
  </channel>
</rss>