<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUboot config folder</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431755#M65712</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there, i am trying to compile and make a custom uboot for imx6 but i see there are two sources:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2014.04_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2014.04_3.14.28_1.0.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;(2) &lt;A href="https://github.com/Freescale/u-boot-fslc" title="https://github.com/Freescale/u-boot-fslc"&gt;Freescale/u-boot-fslc · GitHub&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which one should i use? Also, for (1), there is no "configs" folder that i can modify?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 May 2015 00:48:01 GMT</pubDate>
    <dc:creator>eugenephua</dc:creator>
    <dc:date>2015-05-14T00:48:01Z</dc:date>
    <item>
      <title>Uboot config folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431755#M65712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there, i am trying to compile and make a custom uboot for imx6 but i see there are two sources:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) &lt;A href="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2014.04_3.14.28_1.0.0_ga" title="http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2014.04_3.14.28_1.0.0_ga"&gt;uboot-imx.git - Freescale i.MX u-boot Tree&lt;/A&gt; &lt;/P&gt;&lt;P&gt;(2) &lt;A href="https://github.com/Freescale/u-boot-fslc" title="https://github.com/Freescale/u-boot-fslc"&gt;Freescale/u-boot-fslc · GitHub&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which one should i use? Also, for (1), there is no "configs" folder that i can modify?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 00:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431755#M65712</guid>
      <dc:creator>eugenephua</dc:creator>
      <dc:date>2015-05-14T00:48:01Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot config folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431756#M65713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The u-boot to be used depends on wether you will be using the FSP BSP Release or the FSL Community BSP. There is a bit more information on which layers are included on each on the following document:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-102993"&gt;YOCTO PROJECT LAYERS MIND MAP&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The conf folder is located on the top of each layer, not every individual recipe, or you may use the conf folder on the Build directory for global changes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps! &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 15:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431756#M65713</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-05-14T15:36:14Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot config folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431757#M65714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi gusarambula,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess i am using the FSP BSP Release as i am using the download from &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6SL&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;L3.14.28_1.0.0_iMX6SL_BUNDLE&lt;/A&gt;. So for this case, i should be using the u-boot source from (2)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only change i am making is from the 1GB RAM to 512MB fyi. Hope you can advise, thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2015 01:10:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431757#M65714</guid>
      <dc:creator>eugenephua</dc:creator>
      <dc:date>2015-05-15T01:10:26Z</dc:date>
    </item>
    <item>
      <title>Re: Uboot config folder</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431758#M65715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Correct, you are using the FSL BSP Release so in this case you would be using the second one, which is hosted on git.freescale.com (1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is some information regarding uboot memory configuration on the BSP Porting Guide (attached). &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 May 2015 20:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Uboot-config-folder/m-p/431758#M65715</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-05-21T20:27:30Z</dc:date>
    </item>
  </channel>
</rss>