<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Video output to LCD port - kernel command line in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Video-output-to-LCD-port-kernel-command-line/m-p/175676#M6559</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I try to set up the IPU of an i.MX6Q for putting out the content of framebuffer 0 to the LCD port of the IPU. At the moment, we supply 'video=mxcfb0:dev=lcd,ABC,if=RGB565' to the kernel command line ('ABC' is a string identifying the desired video configuration data which has been added to file mxc_lcdif.c), similar to the LVDS case, which is working fine. Of, course, in addition to that, the framebuffer has been configured using something like 'fbset -fb /dev/fb0 -g 720 480 720 480 16 -t 81584 8 8 8 8 32 36'.&lt;BR /&gt;&lt;BR /&gt;My question is: is this the proper way to setup LCD port output? Is there something missing?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Helmut&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jul 2012 13:20:41 GMT</pubDate>
    <dc:creator>HJahns</dc:creator>
    <dc:date>2012-07-17T13:20:41Z</dc:date>
    <item>
      <title>Video output to LCD port - kernel command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Video-output-to-LCD-port-kernel-command-line/m-p/175676#M6559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I try to set up the IPU of an i.MX6Q for putting out the content of framebuffer 0 to the LCD port of the IPU. At the moment, we supply 'video=mxcfb0:dev=lcd,ABC,if=RGB565' to the kernel command line ('ABC' is a string identifying the desired video configuration data which has been added to file mxc_lcdif.c), similar to the LVDS case, which is working fine. Of, course, in addition to that, the framebuffer has been configured using something like 'fbset -fb /dev/fb0 -g 720 480 720 480 16 -t 81584 8 8 8 8 32 36'.&lt;BR /&gt;&lt;BR /&gt;My question is: is this the proper way to setup LCD port output? Is there something missing?&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;&lt;BR /&gt;Helmut&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2012 13:20:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Video-output-to-LCD-port-kernel-command-line/m-p/175676#M6559</guid>
      <dc:creator>HJahns</dc:creator>
      <dc:date>2012-07-17T13:20:41Z</dc:date>
    </item>
  </channel>
</rss>