<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: MMPF0100 PMIC default configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-PMIC-default-configuration/m-p/430907#M65562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PF0100 PMICs were designed specially for i.MX6 processors&lt;/P&gt;&lt;P&gt;family, this defines default values outputs of PF0100.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Oct 2015 06:31:30 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-10-05T06:31:30Z</dc:date>
    <item>
      <title>MMPF0100 PMIC default configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-PMIC-default-configuration/m-p/430905#M65560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In case of many PMICs, I saw, default output is 0V and they are controled by MCU.&lt;/P&gt;&lt;P&gt;But PF0100 has default configuration for example SW2_VOLT = 3.0V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a reason for default outputs of PF0100?&lt;/P&gt;&lt;P&gt;If default outputs are 0V, they can apply any other systems but it is hard work to do for that reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 00:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-PMIC-default-configuration/m-p/430905#M65560</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2015-10-05T00:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0100 PMIC default configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-PMIC-default-configuration/m-p/430906#M65561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the Section 6.1 of the MMPF0100 Data Sheet document. It clearly says the following.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"The PF0100 can be configured to start-up from either the internal OTP configuration, or with a hard-coded configuration built in to the device. The internal hard-coded configuration is enabled by connecting the VDDOTP pin to VCOREDIG through a 100 kohm resistor. The OTP configuration is enabled by connecting VDDOTP to GND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For NP devices, selecting the OTP configuration causes the PF0100 to not start-up. However, the PF0100 can be controlled through the I2C port for prototyping and programming. Once programmed, the NP device will startup with the customer programmed configuration".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, most likely, you are using a NP device, configured to start up with OTP configuration. Please check.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 05:46:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-PMIC-default-configuration/m-p/430906#M65561</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-10-05T05:46:10Z</dc:date>
    </item>
    <item>
      <title>Re: MMPF0100 PMIC default configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-PMIC-default-configuration/m-p/430907#M65562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JHY&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PF0100 PMICs were designed specially for i.MX6 processors&lt;/P&gt;&lt;P&gt;family, this defines default values outputs of PF0100.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 06:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MMPF0100-PMIC-default-configuration/m-p/430907#M65562</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-05T06:31:30Z</dc:date>
    </item>
  </channel>
</rss>