<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Bitbake returns with error code while making image for imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430597#M65489</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That didn't help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did little more debugging to see what could be. Then I compared the sources directory with the backup I've a while ago. I see below lines changed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;File @ meta-fsl-arm/conf/machine/imx6qsabresd.conf has changes :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Back-up of source:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb"&lt;/P&gt;&lt;P&gt;KERNEL_IMAGETYPE = "zImage"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I removed "imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb" and also KERNEL_IMAGETYPE = "zImage" , from meta-fsl-arm/conf/machine/imx6qsabresd.conf , then it all worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I've not changed them, neither I did "repo sync".&amp;nbsp; Any idea, how would these change?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 17 May 2015 09:36:44 GMT</pubDate>
    <dc:creator>ramprasadvempat</dc:creator>
    <dc:date>2015-05-17T09:36:44Z</dc:date>
    <item>
      <title>Bitbake returns with error code while making image for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430595#M65487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to make image "core-image-base" using bitbake for freescale imx6 platform. Things were working very well. I made image two times as well. But suddently it stopped working. I've used "bitbake core-image-base" command for making build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;below is the error I get. Could someone help me, what must have gone wrong?&lt;/P&gt;&lt;P&gt;'&lt;/P&gt;&lt;P&gt;| make: Leaving directory `/home/ramprasad/fsl-release-bsp-2/build-7/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/image/usr/src/kernel'&lt;/P&gt;&lt;P&gt;| NOTE: make -j 4 imx6q-sabresd.dtb&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.s&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; GEN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.h&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTCC&amp;nbsp; scripts/mod/file2alias.o&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTLD&amp;nbsp; scripts/mod/modpost&lt;/P&gt;&lt;P&gt;| make[1]: `arch/arm/boot/dts/imx6q-sabresd.dtb' is up to date.&lt;/P&gt;&lt;P&gt;| NOTE: make -j 4 imx6q-sabresd-ldo.dtb&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.s&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; GEN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.h&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTCC&amp;nbsp; scripts/mod/file2alias.o&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTLD&amp;nbsp; scripts/mod/modpost&lt;/P&gt;&lt;P&gt;| make[1]: `arch/arm/boot/dts/imx6q-sabresd-ldo.dtb' is up to date.&lt;/P&gt;&lt;P&gt;| NOTE: make -j 4 imx6q-sabresd-hdcp.dtb&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.s&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; GEN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.h&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTCC&amp;nbsp; scripts/mod/file2alias.o&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTLD&amp;nbsp; scripts/mod/modpost&lt;/P&gt;&lt;P&gt;| make[1]: `arch/arm/boot/dts/imx6q-sabresd-hdcp.dtb' is up to date.&lt;/P&gt;&lt;P&gt;| NOTE: make -j 4 imx6q-sabresd-enetirq.dtb&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; CC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.s&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; GEN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; scripts/mod/devicetable-offsets.h&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTCC&amp;nbsp; scripts/mod/file2alias.o&lt;/P&gt;&lt;P&gt;|&amp;nbsp;&amp;nbsp; HOSTLD&amp;nbsp; scripts/mod/modpost&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; | make[1]: *** No rule to make target `arch/arm/boot/dts/imx6q-sabresd-&amp;nbsp; enetirq.dtb'.&amp;nbsp; Stop.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; make: *** [imx6q-sabresd-enetirq.dtb] Error 2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ERROR: oe_runmake failed&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; WARNING: exit code 1 from a shell command.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ERROR: Function failed: do_install (log file is located at&amp;nbsp; /home/ramprasad/fsl-release-bsp-2/build-7/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/3.10.17-r0/temp/log.do_install.11111)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Task 68 (/home/ramprasad/fsl-release-bsp-2/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb, do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 3610 tasks of which 3609 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;No currently running tasks (1718 of 3640)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /home/ramprasad/fsl-release-bsp-2/sources/meta-fsl-arm/recipes-kernel/linux/linux-imx_3.10.17.bb, do_install&lt;/P&gt;&lt;P&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 18:26:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430595#M65487</guid>
      <dc:creator>ramprasadvempat</dc:creator>
      <dc:date>2015-05-13T18:26:56Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake returns with error code while making image for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430596#M65488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ramprasad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it was running correctly and no changes were made perhaps it would help to make a cleanall.&lt;/P&gt;&lt;P&gt;bitbake -c cleanall &amp;lt;IMAGE&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 15:26:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430596#M65488</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2015-05-14T15:26:30Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake returns with error code while making image for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430597#M65489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That didn't help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did little more debugging to see what could be. Then I compared the sources directory with the backup I've a while ago. I see below lines changed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;File @ meta-fsl-arm/conf/machine/imx6qsabresd.conf has changes :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Back-up of source:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Current file:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KERNEL_DEVICETREE = "imx6q-sabresd.dtb imx6q-sabresd-ldo.dtb imx6q-sabresd-hdcp.dtb imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb"&lt;/P&gt;&lt;P&gt;KERNEL_IMAGETYPE = "zImage"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I removed "imx6q-sabresd-enetirq.dtb imx6q-sabresd-uart.dtb" and also KERNEL_IMAGETYPE = "zImage" , from meta-fsl-arm/conf/machine/imx6qsabresd.conf , then it all worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I've not changed them, neither I did "repo sync".&amp;nbsp; Any idea, how would these change?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 May 2015 09:36:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430597#M65489</guid>
      <dc:creator>ramprasadvempat</dc:creator>
      <dc:date>2015-05-17T09:36:44Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake returns with error code while making image for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430598#M65490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After, I pass through above step, I wanted to include dhcp. But I get below error. Any idea how can this be resolved? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: dhcp not found in the base feeds (imx6qsabresd cortexa9hf-vfp-neon-mx6 cortexa9hf-vfp-neon cortexa9hf-vfp armv7ahf-vfp-neon armv7ahf-vfp armv6hf-vfp armv5ehf-vfp armv5hf-vfp noarch any all).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 May 2015 12:25:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430598#M65490</guid>
      <dc:creator>ramprasadvempat</dc:creator>
      <dc:date>2015-05-17T12:25:00Z</dc:date>
    </item>
    <item>
      <title>Re: Bitbake returns with error code while making image for imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430599#M65491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured out answer for above problem. I needed to use "dhcp-client" instead of dhcp. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only puzzling thing is, how did my "imx6qsabresd.conf" changed on it's own.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the problem in this thread is resolved. So I will be marking it as "Answered"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 May 2015 13:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Bitbake-returns-with-error-code-while-making-image-for-imx6/m-p/430599#M65491</guid>
      <dc:creator>ramprasadvempat</dc:creator>
      <dc:date>2015-05-17T13:04:01Z</dc:date>
    </item>
  </channel>
</rss>