<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.mx6 HDMI without I2C in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430459#M65469</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please create new thread, as this is new problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Sep 2015 06:54:06 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-09-08T06:54:06Z</dc:date>
    <item>
      <title>i.mx6 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430453#M65463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am currently trying to enable the HDMI display on the i.mx6 quad CPU.&lt;/P&gt;&lt;P&gt;May i know whether the HDMI_TX_DDC_SCL and HDMI_TX_DDC_SDA pin connection is mandatory in order for the HDMI core to function? I see that in the driver drivers/video/mxc_hdmi.c, there are a lot of configurations that is related to i2c communication. What will happen if i did not connect out both the HDMI SCL and SDA pin?&lt;/P&gt;&lt;P&gt;By the way, I do not need to configure any setting on the HDMI display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;ZC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Sep 2015 08:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430453#M65463</guid>
      <dc:creator>zc_tee</dc:creator>
      <dc:date>2015-09-07T08:03:42Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430454#M65464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can work with i.MX6 HDMI without using HDMI SCL and SDA or&lt;/P&gt;&lt;P&gt;using ordinary I2C signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Sep 2015 11:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430454#M65464</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-07T11:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430455#M65465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Igor,&lt;/P&gt;&lt;P&gt;Thanks for reply,&lt;/P&gt;&lt;P&gt;Just for confirmation, does it means that I MUST connect at least one I2C port (be it HDMI I2C or ordinary I2C) to the HDMI display in order for the HDMI to work?&lt;/P&gt;&lt;P&gt;What will happen if the I2C port of the HDMI display is left unconnected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;ZC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 00:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430455#M65465</guid>
      <dc:creator>zc_tee</dc:creator>
      <dc:date>2015-09-08T00:51:03Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430456#M65466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You may set HDMI in DVI mode.&lt;/P&gt;&lt;P&gt;Also, it will be needed to add the new 'allow_noncea=1' environment variable in the U-Boot &lt;BR /&gt;configuration and the proper arguments for display resolution to the kernel command line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 02:26:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430456#M65466</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-09-08T02:26:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430457#M65467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;no, it does not mean that one must to connect at least one I2C port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 02:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430457#M65467</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-08T02:39:58Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430458#M65468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;Currently i facing problem where i cannot get the HPD interrupt.&lt;/P&gt;&lt;P&gt;I checked the hardware signal, when plugged in, the HPD pin is HI, and when plugged out, the HPD pin is LO.&lt;/P&gt;&lt;P&gt;However, kernel does not goes in to irq routine mxc_hdmi_hotplug, and also not going in to hotplug_worker at all.&lt;/P&gt;&lt;P&gt;Any idea why is this happening? i am using kernel BSP 3.0.101. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;ZC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 04:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430458#M65468</guid>
      <dc:creator>zc_tee</dc:creator>
      <dc:date>2015-09-08T04:29:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx6 HDMI without I2C</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430459#M65469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ZC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please create new thread, as this is new problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 06:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx6-HDMI-without-I2C/m-p/430459#M65469</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-08T06:54:06Z</dc:date>
    </item>
  </channel>
</rss>