<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: SabreAuto UART Configuration</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SabreAuto-UART-Configuration/m-p/430198#M65442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exact the same issue.&lt;/P&gt;&lt;P&gt;I do not find where the above two constants are defined in the u-boot source code.&lt;/P&gt;&lt;P&gt;It looks like a miracle that it compiled fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit, Ok, according to the definition of MX6_PAD_DECL every thing is clear now.&lt;/P&gt;&lt;P&gt;There exists a definition for MX6_PAD_DECL(KEY_COL0__UART4_TX_DATA.... which is basically creating the constant i was looking for.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 May 2016 08:56:36 GMT</pubDate>
    <dc:creator>mamsadegh</dc:creator>
    <dc:date>2016-05-30T08:56:36Z</dc:date>
    <item>
      <title>SabreAuto UART Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreAuto-UART-Configuration/m-p/430197#M65441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to reconfigure our custom board based upon the SabreAuto (iMX6Q) to use a different UART for serial console for u-boot and Linux.&amp;nbsp; I have been unable to locate any real instructions on how this can be accomplished but have derived a lot of it by reading the processor manuals and examining code.&amp;nbsp; I have been unable to locate some of the definitions in the code even with exhaustive searching. Specifically, I cannot find the following definitions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MX6_PAD_KEY_COL0__UART4_TX_DATA&lt;/P&gt;&lt;P&gt;MX6_PAD_KEY_ROW0__UART4_RX_DATA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone point out where I can find these symbols and also some better instructions on how to reconfigure U-Boot/Linux to a different set of PADS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Oct 2015 19:29:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreAuto-UART-Configuration/m-p/430197#M65441</guid>
      <dc:creator>cbrust</dc:creator>
      <dc:date>2015-10-26T19:29:15Z</dc:date>
    </item>
    <item>
      <title>Re: SabreAuto UART Configuration</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SabreAuto-UART-Configuration/m-p/430198#M65442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have exact the same issue.&lt;/P&gt;&lt;P&gt;I do not find where the above two constants are defined in the u-boot source code.&lt;/P&gt;&lt;P&gt;It looks like a miracle that it compiled fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit, Ok, according to the definition of MX6_PAD_DECL every thing is clear now.&lt;/P&gt;&lt;P&gt;There exists a definition for MX6_PAD_DECL(KEY_COL0__UART4_TX_DATA.... which is basically creating the constant i was looking for.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 May 2016 08:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SabreAuto-UART-Configuration/m-p/430198#M65442</guid>
      <dc:creator>mamsadegh</dc:creator>
      <dc:date>2016-05-30T08:56:36Z</dc:date>
    </item>
  </channel>
</rss>