<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PF0200 OTP programming problem in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429830#M65342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;Thank you for verifying the programming file. We follow the exact same step as you outline.&lt;/P&gt;&lt;P&gt;The OTP programming is reported successful ("verify after programming" is enabled) but when we do a blank check afterwards it is reported blank. If the settings are retrieved/extracted from the PMIC it reports the correct values but after a power cycle the values are gone (all are 0x00).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="prog_fail1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55689i2F579E3A2DEA7B50/image-size/large?v=v2&amp;amp;px=999" role="button" title="prog_fail1.png" alt="prog_fail1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2015 09:40:00 GMT</pubDate>
    <dc:creator>andersrosvall</dc:creator>
    <dc:date>2015-07-22T09:40:00Z</dc:date>
    <item>
      <title>PF0200 OTP programming problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429827#M65339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have an unprogrammed PF0200 PMIC on a new iMX6 design that I'm working on.&lt;/P&gt;&lt;P&gt;There is a connector on the board so that it is possible to program the PMIC via Freescale's "PF Series Programmer". I have followed the guidelines in the application note for on-board OTP programming. I have a rev B programmer and use the ver 4 GUI application.&lt;/P&gt;&lt;P&gt;I can download settings in TBB mode and everything works as it should... but I cannot program the OTP fuses and get the PMIC to start up with the values I have programmed.&lt;/P&gt;&lt;P&gt;When I program the OTP fuses via the GUI everything seems ok. I can read back the correct values but as soon as the PMIC is power cycled the previously programmed values are gone.&lt;/P&gt;&lt;P&gt;I think it all boils down to the "FUSE_POR_XOR"&amp;nbsp; bit in register 0xE7 (reg bank 1). This bit is always zero. I cannot get this bit to be set.&lt;/P&gt;&lt;P&gt;If I 'blank check' the PMIC after programming, the GUI reports that the device is blank, but when I checked with a logic analyzer that the GUI really does when 'blank checking' I saw that it just reads the "FUSE_POR_XOR"&amp;nbsp; bit in register 0xE7.&lt;/P&gt;&lt;P&gt;I have attached the programming script I use.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas what the problem can be? Things to check?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Anders&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335801"&gt;Example_Script-(F6-Sample-ManualProgramECC).txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 16:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429827#M65339</guid>
      <dc:creator>andersrosvall</dc:creator>
      <dc:date>2015-07-21T16:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: PF0200 OTP programming problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429828#M65340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Anders,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I will discuss your question with Power AE team, please wait some time ...!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 07:10:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429828#M65340</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2015-07-22T07:10:25Z</dc:date>
    </item>
    <item>
      <title>Re: PF0200 OTP programming problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429829#M65341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anders,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; We did test, and see the following reply from Power AE team:&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;With the customer script, I can program well. So this is not the script problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;The only one thing is there is an error after programming, please add a line as below. Of course this error will not impact the OTP result.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;WRITE_I2C:7F:01 // Access FSL EXT Page 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; background: yellow;"&gt;WRITE_I2C:FF:08 // I2C Device Address = 0x08&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;I’d like to check with the customer their operating steps, if the steps are the same, I think this should be the board problem.&lt;/SPAN&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;1.&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;Enable Target&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;2.&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;Go to Programming tab&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;3.&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;Select Programming Script File in DATA SOURCE panel, then click&amp;nbsp; Get Input button to get the script&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;4.&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;Click Convert Script File on the bottom to convert the script file into a good format&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;5.&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;Check Verify After Programming button in PROGRAMMING panel&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;6.&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;Click PROGRAM button to start programming. If programming correct, it will tell there is no error in log&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;7.&lt;/SPAN&gt; &lt;SPAN style="color: #1f497d;"&gt;Click black Check button, it says DEVICE PROGRAMMED &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="status.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55360i9DB08A33D1460742/image-size/large?v=v2&amp;amp;px=999" role="button" title="status.png" alt="status.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 08:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429829#M65341</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2015-07-22T08:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: PF0200 OTP programming problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429830#M65342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Weidong,&lt;/P&gt;&lt;P&gt;Thank you for verifying the programming file. We follow the exact same step as you outline.&lt;/P&gt;&lt;P&gt;The OTP programming is reported successful ("verify after programming" is enabled) but when we do a blank check afterwards it is reported blank. If the settings are retrieved/extracted from the PMIC it reports the correct values but after a power cycle the values are gone (all are 0x00).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="prog_fail1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55689i2F579E3A2DEA7B50/image-size/large?v=v2&amp;amp;px=999" role="button" title="prog_fail1.png" alt="prog_fail1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 09:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429830#M65342</guid>
      <dc:creator>andersrosvall</dc:creator>
      <dc:date>2015-07-22T09:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: PF0200 OTP programming problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429831#M65343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just to wrap things up (in case someone else run into this problem) - the problem is that if pin 56 (PWRON) is held low by an external source then programming will fail and the programming GUI will not give any error indication.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Sep 2015 09:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/PF0200-OTP-programming-problem/m-p/429831#M65343</guid>
      <dc:creator>andersrosvall</dc:creator>
      <dc:date>2015-09-10T09:58:32Z</dc:date>
    </item>
  </channel>
</rss>