<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: IMX28 with USB Wiggler</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429565#M65288</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You have to configure boot pins for JTAG boot mode (DEBUG is LOW for Bondary Scan, &lt;BR /&gt;HIGH for software debug) and provide POR (power on sequence). Please refer to Table 12-3 &lt;BR /&gt;(Boot Mode Selection Map) of the i.MX28 Reference Manual. After that You may start up JTAG &lt;BR /&gt;testing.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Oct 2015 06:42:34 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-10-02T06:42:34Z</dc:date>
    <item>
      <title>IMX28 with USB Wiggler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429564#M65287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying to bringup Freescale IMX28 processor using USB Wiggler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configured LCD_D01, LCD_D02, LCD_RS pins are pulled high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Interfaced the USB Wiggler with IMX28 processor,&lt;/P&gt;&lt;P&gt;We are getting the following error while trying to connect using USB Wiggler.&lt;/P&gt;&lt;P&gt;sudo ocdremote -c iMX28 -d USB -a 0 -s 2&lt;/P&gt;&lt;P&gt;OCDemon InitializeTarget Error : Cable Disconnected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We confirmed that POWER, RESET, CLOCK pins are fine. Also tried with DEBUG pin configured as Pulled High &amp;amp; Low as well.&lt;/P&gt;&lt;P&gt;Please share your inputs in this regards,&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hariharan.V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2015 05:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429564#M65287</guid>
      <dc:creator>neeveehariharan</dc:creator>
      <dc:date>2015-10-02T05:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 with USB Wiggler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429565#M65288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; You have to configure boot pins for JTAG boot mode (DEBUG is LOW for Bondary Scan, &lt;BR /&gt;HIGH for software debug) and provide POR (power on sequence). Please refer to Table 12-3 &lt;BR /&gt;(Boot Mode Selection Map) of the i.MX28 Reference Manual. After that You may start up JTAG &lt;BR /&gt;testing.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2015 06:42:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429565#M65288</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-02T06:42:34Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 with USB Wiggler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429566#M65289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We applied the POR ( Power on Reset ) sequence properly.&lt;/P&gt;&lt;P&gt;Please help me to configure DEBUG pin, whether it needs to Pulled LOW or HIGH for using USB Wiggler JTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hariharan.V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Oct 2015 13:29:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429566#M65289</guid>
      <dc:creator>neeveehariharan</dc:creator>
      <dc:date>2015-10-04T13:29:46Z</dc:date>
    </item>
    <item>
      <title>Re: IMX28 with USB Wiggler</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429567#M65290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; For software debugging : &lt;/P&gt;&lt;P&gt;LCD_D04 = 0&lt;/P&gt;&lt;P&gt;LCD_D03 = 0&lt;BR /&gt;LCD_D02 = 1&lt;BR /&gt;LCD_D01 = 1 &lt;BR /&gt;LCD_D00 = 0&lt;/P&gt;&lt;P&gt;DEBUG = 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Table 12-3 (Boot Mode Selection Map) of i.MX28 RM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 03:30:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-with-USB-Wiggler/m-p/429567#M65290</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-10-05T03:30:22Z</dc:date>
    </item>
  </channel>
</rss>