<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR stress test fail in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-fail/m-p/429424#M65256</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bill&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems problem with bit 28, "0x10000000" it may be poorly&lt;/P&gt;&lt;P&gt;soldered or shorted with other signal. Recommended to check it with&lt;/P&gt;&lt;P&gt;oscilloscope. Also had you tried older version v.1.03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-96412"&gt;i.MX6 DDR Stress Test Tool V1.0.3&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Oct 2015 07:54:16 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-10-02T07:54:16Z</dc:date>
    <item>
      <title>DDR stress test fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-fail/m-p/429423#M65255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Design platform: i.MX6 DL 1GHz&lt;/P&gt;&lt;P&gt;RAM: LPDDR2 1GB, 2 chip in 1 die, @396Hz&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When i tried to run the Stress test v2.20&lt;/P&gt;&lt;P&gt;and no matter i ran at 352MHz, 396MHz, and 413MHz,&lt;/P&gt;&lt;P&gt;after several tens loops (it can pass stress test, but it will also fail), failure occurs at all these frequency with same errors report &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DDR Freq: 413 MHz&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;/P&gt;&lt;P&gt;t0: memcpy11 SSN test&lt;/P&gt;&lt;P&gt;t1: memcpy8 SSN test&lt;/P&gt;&lt;P&gt;t2: byte-wise SSN test&lt;/P&gt;&lt;P&gt;t3: memcpy11 random pattern test&lt;/P&gt;&lt;P&gt;test3 Address:&amp;nbsp;&amp;nbsp; 0x2400c944&lt;/P&gt;&lt;P&gt;Data read was:&amp;nbsp;&amp;nbsp; 0x358bf292&lt;/P&gt;&lt;P&gt;But pattern was: 0x258bf292&lt;/P&gt;&lt;P&gt;Bit location:&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10000000&lt;/P&gt;&lt;P&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DDR Stress Test Iteration 34&lt;/P&gt;&lt;P&gt;Current Tempareture: 64&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;DDR Freq: 352 MHz&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;/P&gt;&lt;P&gt;t0: memcpy11 SSN test&lt;/P&gt;&lt;P&gt;t1: memcpy8 SSN test&lt;/P&gt;&lt;P&gt;t2: byte-wise SSN test&lt;/P&gt;&lt;P&gt;t3: memcpy11 random pattern test&lt;/P&gt;&lt;P&gt;test3 Address:&amp;nbsp;&amp;nbsp; 0x2400c944&lt;/P&gt;&lt;P&gt;Data read was:&amp;nbsp;&amp;nbsp; 0x358bf292&lt;/P&gt;&lt;P&gt;But pattern was: 0x258bf292&lt;/P&gt;&lt;P&gt;Bit location:&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10000000&lt;/P&gt;&lt;P&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DDR Stress Test Iteration 36&lt;/P&gt;&lt;P&gt;Current Tempareture: 64&lt;/P&gt;&lt;P&gt;============================================&lt;/P&gt;&lt;P&gt;DDR Freq: 396 MHz&lt;/P&gt;&lt;P&gt;t0.1: data is addr test&lt;/P&gt;&lt;P&gt;t0: memcpy11 SSN test&lt;/P&gt;&lt;P&gt;t1: memcpy8 SSN test&lt;/P&gt;&lt;P&gt;t2: byte-wise SSN test&lt;/P&gt;&lt;P&gt;t3: memcpy11 random pattern test&lt;/P&gt;&lt;P&gt;test3 Address:&amp;nbsp;&amp;nbsp; 0x2400c944&lt;/P&gt;&lt;P&gt;Data read was:&amp;nbsp;&amp;nbsp; 0x358bf292&lt;/P&gt;&lt;P&gt;But pattern was: 0x258bf292&lt;/P&gt;&lt;P&gt;Bit location:&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10000000&lt;/P&gt;&lt;P&gt;Error: failed to run stress test!!!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, the failure always occurs at &lt;/P&gt;&lt;P&gt;t3: memcpy11 random pattern test&lt;/P&gt;&lt;P&gt;test3 Address:&amp;nbsp;&amp;nbsp; 0x2400c944&lt;/P&gt;&lt;P&gt;Data read was:&amp;nbsp;&amp;nbsp; 0x358bf292&lt;/P&gt;&lt;P&gt;But pattern was: 0x258bf292&lt;/P&gt;&lt;P&gt;Bit location:&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x10000000&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anyone&amp;nbsp; have an idea what has gone wrong?&lt;/P&gt;&lt;P&gt;i can see bit location 0x10000000 got a problem, is it something related to chip 0 and chip 1 selection or switching ?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I attached one of the stress test log and the inc we used.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336977"&gt;ddr_stresstest_20151002-11'4'32.log.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336977"&gt;lpddr2.inc.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2015 03:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-fail/m-p/429423#M65255</guid>
      <dc:creator>billlau</dc:creator>
      <dc:date>2015-10-02T03:33:14Z</dc:date>
    </item>
    <item>
      <title>Re: DDR stress test fail</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-fail/m-p/429424#M65256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bill&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;seems problem with bit 28, "0x10000000" it may be poorly&lt;/P&gt;&lt;P&gt;soldered or shorted with other signal. Recommended to check it with&lt;/P&gt;&lt;P&gt;oscilloscope. Also had you tried older version v.1.03&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-96412"&gt;i.MX6 DDR Stress Test Tool V1.0.3&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Oct 2015 07:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/DDR-stress-test-fail/m-p/429424#M65256</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-10-02T07:54:16Z</dc:date>
    </item>
  </channel>
</rss>