<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI slave detection in linux userspace in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-slave-detection-in-linux-userspace/m-p/429389#M65252</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Srinivasa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach some spi device like spi-nor or adc/dac and test it, preferably checking&lt;/P&gt;&lt;P&gt;signals with oscilloscope, like described below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/309866"&gt;i.MX6 ECSPI single burst transfers&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Sep 2015 02:03:20 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2015-09-07T02:03:20Z</dc:date>
    <item>
      <title>SPI slave detection in linux userspace</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-slave-detection-in-linux-userspace/m-p/429388#M65251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have got a Freescale's IMX6DL reference board (Wandboard Dual). We have ported Ubuntu to this and able to boot successfully. Now we would like interface some other modules to this board externally through SPI. We have made entry for spi module in device tree and when we are booting we could able to see /dev/spidev0.0. And also we checked with spi_test.c program which is confirming that the board is working as spi master (spi is working correctly) by shorting MOSI and MISO pins in JP4. But how we can check the correctness of SPI slave devices correctly. Whether that hardware working or not, connections are correct etc. how we will come to know about spi slave devices connected.. in the linux user space.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 Sep 2015 10:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-slave-detection-in-linux-userspace/m-p/429388#M65251</guid>
      <dc:creator>srinivasaraopor</dc:creator>
      <dc:date>2015-09-06T10:30:12Z</dc:date>
    </item>
    <item>
      <title>Re: SPI slave detection in linux userspace</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-slave-detection-in-linux-userspace/m-p/429389#M65252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Srinivasa&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can attach some spi device like spi-nor or adc/dac and test it, preferably checking&lt;/P&gt;&lt;P&gt;signals with oscilloscope, like described below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/309866"&gt;i.MX6 ECSPI single burst transfers&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Sep 2015 02:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-slave-detection-in-linux-userspace/m-p/429389#M65252</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-09-07T02:03:20Z</dc:date>
    </item>
  </channel>
</rss>