<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックQuestion, i.MX28 clock input</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-clock-input/m-p/429378#M65249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about i.MX28 clock input.&lt;/P&gt;&lt;P&gt;My customer has started the HW design for their own i.MX28 board and they will use crystal for i.MX28 clock input.&lt;/P&gt;&lt;P&gt;Do you have any specification for clock input?&lt;/P&gt;&lt;P&gt;Duty cycles, deflection voltage range, etc.&lt;/P&gt;&lt;P&gt;The customer is trying to use a crystal which has about 560mV of deflection range.&lt;/P&gt;&lt;P&gt;Is it OK for i.MX28?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Nov 2015 03:38:32 GMT</pubDate>
    <dc:creator>Aemj</dc:creator>
    <dc:date>2015-11-20T03:38:32Z</dc:date>
    <item>
      <title>Question, i.MX28 clock input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-clock-input/m-p/429378#M65249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask about i.MX28 clock input.&lt;/P&gt;&lt;P&gt;My customer has started the HW design for their own i.MX28 board and they will use crystal for i.MX28 clock input.&lt;/P&gt;&lt;P&gt;Do you have any specification for clock input?&lt;/P&gt;&lt;P&gt;Duty cycles, deflection voltage range, etc.&lt;/P&gt;&lt;P&gt;The customer is trying to use a crystal which has about 560mV of deflection range.&lt;/P&gt;&lt;P&gt;Is it OK for i.MX28?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Miyamoto&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 03:38:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-clock-input/m-p/429378#M65249</guid>
      <dc:creator>Aemj</dc:creator>
      <dc:date>2015-11-20T03:38:32Z</dc:date>
    </item>
    <item>
      <title>Re: Question, i.MX28 clock input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-clock-input/m-p/429379#M65250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The i.MX28 processor has the internal oscillation circuits for both 32kHz and 24MHz clock sources. Both oscillation circuits are supplied from the internal linear voltage regulator that produces the VDDXTAL voltage whose typical value is 1.1V. The typical external crystal parameters are as per the specifications attached. The typical duty cycle is 50%.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Artur&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Nov 2015 09:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Question-i-MX28-clock-input/m-p/429379#M65250</guid>
      <dc:creator>art</dc:creator>
      <dc:date>2015-11-24T09:27:40Z</dc:date>
    </item>
  </channel>
</rss>