<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Gplay options via command line</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428674#M65130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please look at the enclosed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2015 06:55:36 GMT</pubDate>
    <dc:creator>Yuri</dc:creator>
    <dc:date>2015-08-11T06:55:36Z</dc:date>
    <item>
      <title>Gplay options via command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428673#M65129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am keen to know if gplay has command line options to set the volume or to mute.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i do gplay --help on command prompt, only&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gplay file_list&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is shown.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when i play using gplay sample.mp3,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i get options to pause,play,stop,mute etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My intention is to control the options via command line at the command gplay execution itself not while it is playing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 06:13:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428673#M65129</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-08-11T06:13:35Z</dc:date>
    </item>
    <item>
      <title>Re: Gplay options via command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428674#M65130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Please look at the enclosed.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yuri&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 06:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428674#M65130</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-11T06:55:36Z</dc:date>
    </item>
    <item>
      <title>Re: Gplay options via command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428675#M65131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yuri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Last line in chapter 1 says&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customers can operate the player through pressing keys from keyboard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's my question.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can we do it in one shot. say for example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gplay sample.mp3 -v 100%&amp;nbsp; or something like that to change the volume to 100%&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gplay sample.mp3 -m to mute&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Above are just examples that i would like to have as a user.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something like that??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Manju&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 07:15:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428675#M65131</guid>
      <dc:creator>manjunathjoshi</dc:creator>
      <dc:date>2015-08-11T07:15:25Z</dc:date>
    </item>
    <item>
      <title>Re: Gplay options via command line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428676#M65132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; You may try to use standard Linux features. As an example :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;$ (echo "key_A" ; sleep 5 ; echo "key_B") | gplay "file_name" &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Yuri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 07:48:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gplay-options-via-command-line/m-p/428676#M65132</guid>
      <dc:creator>Yuri</dc:creator>
      <dc:date>2015-08-11T07:48:38Z</dc:date>
    </item>
  </channel>
</rss>