<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックGstreamer-1.x and FSL plugins with Linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-1-x-and-FSL-plugins-with-Linux-kernel-3-0-35-from-LTIB/m-p/428203#M65055</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working with MX6Q and Ltib L3.0.35_4.1.0.&lt;/P&gt;&lt;P&gt;The gstreamer included in L3.0.35_4.1.0 is 0.1x and I would like to switch to gstreamer-1.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems that fsl-L3.14.28_1.0.0_iMX6qdls_Bundle comes with gstreamer-1.x.&lt;/P&gt;&lt;P&gt;But I do not want to change my kernel and drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So is there a way to use gstreamer-1.x and the corresponding FSL video plugins with linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Robbie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jun 2015 14:52:36 GMT</pubDate>
    <dc:creator>RobbieJiang</dc:creator>
    <dc:date>2015-06-24T14:52:36Z</dc:date>
    <item>
      <title>Gstreamer-1.x and FSL plugins with Linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-1-x-and-FSL-plugins-with-Linux-kernel-3-0-35-from-LTIB/m-p/428203#M65055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm currently working with MX6Q and Ltib L3.0.35_4.1.0.&lt;/P&gt;&lt;P&gt;The gstreamer included in L3.0.35_4.1.0 is 0.1x and I would like to switch to gstreamer-1.x.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems that fsl-L3.14.28_1.0.0_iMX6qdls_Bundle comes with gstreamer-1.x.&lt;/P&gt;&lt;P&gt;But I do not want to change my kernel and drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So is there a way to use gstreamer-1.x and the corresponding FSL video plugins with linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Robbie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jun 2015 14:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-1-x-and-FSL-plugins-with-Linux-kernel-3-0-35-from-LTIB/m-p/428203#M65055</guid>
      <dc:creator>RobbieJiang</dc:creator>
      <dc:date>2015-06-24T14:52:36Z</dc:date>
    </item>
    <item>
      <title>Re: Gstreamer-1.x and FSL plugins with Linux kernel 3.0.35( from LTIB L3.0.35_4.1.0)?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-1-x-and-FSL-plugins-with-Linux-kernel-3-0-35-from-LTIB/m-p/428204#M65056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robbie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid this is not possible, since plugins are compiled for&lt;/P&gt;&lt;P&gt;specific kernel, as discussed below&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-93387"&gt;GStreamer i.MX6 Pipelines&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;igor&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 02:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Gstreamer-1-x-and-FSL-plugins-with-Linux-kernel-3-0-35-from-LTIB/m-p/428204#M65056</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2015-06-25T02:52:40Z</dc:date>
    </item>
  </channel>
</rss>