<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Imx6 Sabrilite not receiving Packets</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx6-Sabrilite-not-receiving-Packets/m-p/427149#M64804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is resolved. This issue is due to J6 Packing VLAN Tag with its ethernet Packets&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Sarah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 May 2015 11:48:49 GMT</pubDate>
    <dc:creator>sarahblessie</dc:creator>
    <dc:date>2015-05-14T11:48:49Z</dc:date>
    <item>
      <title>Imx6 Sabrilite not receiving Packets</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6-Sabrilite-not-receiving-Packets/m-p/427148#M64803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a imx6 sabrelite board and I am trying to ping the boards IP from the PC and It works fine, similarly I could ping PC from the imx6 board.&lt;/P&gt;&lt;P&gt;I have a Vayu EVM board and I trying to ping this board from the imx6 and it could not and the same when tried other way.&lt;/P&gt;&lt;P&gt;this is my result when tried ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ping form imx6&lt;/P&gt;&lt;P&gt; ping 172.16.7.117&lt;/P&gt;&lt;P&gt;PING 172.16.7.117 (172.16.7.117): 56 data bytes&lt;/P&gt;&lt;P&gt;^C&lt;/P&gt;&lt;P&gt;--- 172.16.7.117 ping statistics ---&lt;/P&gt;&lt;P&gt;3484 packets transmitted, 0 packets received, 100% packet loss&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ping from j6&lt;/P&gt;&lt;P&gt;ping 172.16.7.123&lt;/P&gt;&lt;P&gt;PING 172.16.7.123 (172.16.7.123): 56 data bytes&lt;/P&gt;&lt;P&gt;^C&lt;/P&gt;&lt;P&gt;--- 172.16.7.123 ping statistics ---&lt;/P&gt;&lt;P&gt;2941 packets transmitted, 0 packets received, 100% packet loss&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No reply packets are received,&lt;/P&gt;&lt;P&gt;I also tried sending ethernet and IP packets from imx6 on multicast and could successfully receive in the Vayu board. But when the Vayu board sends the packet the imx socket could not receive. But the same packets from PC could be received by imx6.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest me of solution! Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sarah Blessie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2015 08:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6-Sabrilite-not-receiving-Packets/m-p/427148#M64803</guid>
      <dc:creator>sarahblessie</dc:creator>
      <dc:date>2015-05-13T08:04:10Z</dc:date>
    </item>
    <item>
      <title>Re: Imx6 Sabrilite not receiving Packets</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6-Sabrilite-not-receiving-Packets/m-p/427149#M64804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is resolved. This issue is due to J6 Packing VLAN Tag with its ethernet Packets&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Sarah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 11:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6-Sabrilite-not-receiving-Packets/m-p/427149#M64804</guid>
      <dc:creator>sarahblessie</dc:creator>
      <dc:date>2015-05-14T11:48:49Z</dc:date>
    </item>
  </channel>
</rss>